Other Parts Discussed in Thread: BQ500211 Hi,
I am designing the Transmitter & receiver Module by using Solar power circuit / usb power as the input to the transmitter. I am having the below queries at designing stage. Please clarify,
1. U sing the FOD…
Other Parts Discussed in Thread: BQ500412EVM-584 , BQ500410A , BQ500412 , BQ500210 , BQ500212AEVM-550 , BQ500212 , BQ500211 , BQ500211A Greetings,
This is Víctor Mayoral, a researcher at the center for Micro BioRobotics at the Italian Institute of Technology…
Other Parts Discussed in Thread: BQ51013B , BQ500211A , BQ51013BEVM-764 Hello, all
Now we have one inquiry regarding power supply between bq500211A and bq51013B from our customer.
They are evaluating their own design board which is based on BQ500211AEVM-210…
Q1 -- May I know what is the maximum current of BUZ_AC and BUZ_DC can be supplied to drive the buzzer ?
A1 – 4mA
Q2 -- What is the purpose of 10K resistor connected from BUZ_AC to GND ?
A2 – The bq500211AEVM-210 has a 10k resisotor (R45) across…
Other Parts Discussed in Thread: BQ51013BEVM-764 , BQ51013B Hi, I recently acquired bq500211AEVM-210 and BQ51013BEVM-764 but they doesn't seem to be working. I've connected the transmitter to a DC-source that supplies 5V and around 35mA to the transmitter…
hopefully this isn't too simplistic a question but I'm not getting something that seems fundamental....
using the EVMs noted out of the box and without modification, I'm trying to set up a measurement. instead of electronic load we are using…
Other Parts Discussed in Thread: BQ500210 , BQ500212A
3146.bqTESLA TX Sleep Mode -- MSP430 Based.pdf
The bqTESLA Transmitter (TX) will use Sleep Mode to reduce input power when no Receiver (RX) is present. We have two methods for doing this one is MSP430…
hi all.
I’m using bq51050 for new design..
I have several questions...
in the datasheet page 25 equation number 5.. "is to be placed on top of this surface and the inductance is to be measured at 1-V RMS and a frequency of 100 kHz. This measurement…