Part Number: BQ500212A Other Parts Discussed in Thread: BQ51013C Tool/software: Dear Sr.
I would like your recomendation about the best parts to be used in a new design complying the standard WPC v2.0
The system manage a power of 3W.
Thanks in advance…
Hello
Sorry but unfortunately the BQ500212A is Not Recommended for New Designs, no replacement for wireless power TX. Support for this device is not available.
Part Number: BQ500212A Hi Expert,
Since BQ500212A is NRND, do we have new similar wireless transmitter device? Also do we have automotive device? It would be great that you can send me the roadmap. Thanks!
BR,
Elec Cheng
Hello
Double check the connection to pin 35 of BQ500212A. It looks like 3.3V is connected to the pin.
This is 1.8V internal core voltage and should have capacitive divider connected to it, 1uF to gnd and 1uF to 3.3V. A 2.2uF will work also. Trying…
Part Number: BQ500212A Other Parts Discussed in Thread: BQ51050B Hi team,
Customer is searching a wireless charging solution that can support Qi and constant communication during charging. I was wondering if BQ51050B and BQ500212A can work. Besides…
Part Number: BQ500212A Other Parts Discussed in Thread: BQ51013B-Q1 Hi, I need to know if your wireless charging IC has low latency communication through induced charging. In addition to loading, is it possible to send a personalized message by me between…
Hello
The BQ500212A and all other TI wireless power transmitters are NRND. We have no plans to End of Life the units and they will be available for a long time.
Any Qi certified transmitter design would work with the BQ51013B.
Note that the TYLT…
Part Number: BQ500212A Other Parts Discussed in Thread: BQ51050B I have to design a new product which should be based on the BQ500212A but it's end of life. I am using the BQ51050B receiver and would like to know which transmitter should be used.
Regards…
Part Number: BQ500212A According to the I2C interface note, there is a control error byte in block 0xD0. As noted, it is updated frequently. When a device is charging steadily it seems to be switching between 8 and 9. The device I'm working on is having…