Hi TJ
The address is 0x6C
We have not had problems with the address it is the same on bq51021 and ba51025 and bq510221 also.
Also the BQ5102X EVM GUI may be help in debugging the problem.
www.ti.com/.../sluc575
Hello
The BQ51020 (WPC) or BQ51021(WPC) are better alternatives to the BQ51221(WPC+PMA). They have similar pin out and will fit the TIDA-00243 form factor. The 020 and 021 will support WPC only. Units have been certified to WPC 1.2 standard.
Hello
The BQ51021 has I2C interface and the option to send data to the transmitter. For this approach you will also need an transmitter that can support this function. The BQ500212A has I2C.
Sorry do not have info on coil that will act as NFC and…
Other Parts Discussed in Thread: BQ25896 , BQ51021 Dear BMS team,
Does the bq25896 allow operation from wireless charging input ?
More precisely, I would connect the output of bq51021 to the charger input pin (VBUS) of bq25896.
thanks
Paul
The BQ51222 is a dual mode WPC and PMA device.
If only WPC (Qi) is needed then a better solution is the BQ51020 or BQ51021. EVMs are typically available for Digikey or Mouser also contact local TI representative.
Son,
Are you interested in the receiver or transmitter displaying charge status? The transmitter (bq500511A) would need to get that information from the receiver. If it's a display on the phone, then that information does not need to go to the transmitter…
Hi Janith
For data transfer RX to TX it may be possible to used the Proprietary Packet option of the bq51021 Receiver to send info to bq500215 TX. This would require I2C communications with both RX and TX.
Other Parts Discussed in Thread: BQ51021 , BQ51020 , BQ25100 , BQ51025 , BQ24250 , BQ51051B , BQ51050B For space reason in my application, I need to connect the antenna to his corresponding device, BQ51021 with a cable of 7 m long, does't work?
Other Parts Discussed in Thread: BQ51021 , BQ51221 , BQ501210 , BQ500212A I'm working on a project that will require the wireless receiver to identify the charging station it's interfacing for power. The Qi wireless power transfer specification states…