Part Number: BQ769142 Tool/software: Hi All,
can you confirm that CFETOFF, DFETOFF and FET control commands (CHG_PCHG_OFF, DSG_PDSG_OFF) override the body diode protection activation?
Using the I2C commands and driving the input signals (e.g. CFETOFF…
Part Number: BQ769142 Other Parts Discussed in Thread: BQ34Z100-R2 , EV2400 , MKST-3P-ALT-EV2300 Tool/software: Dear all,
can you please give me exact hints and directions to the production tools available from your side for end-of-line programming…
Part Number: BQ769142 Tool/software: Dear Technical support,
in the datasheet of BQ769142, chapter 2 Applications is listed "Non-military drones": what does it means?
In the document "TI’s commitment to defense and aerospace customers" (sszt034.pdf…
Part Number: BQ769142 Other Parts Discussed in Thread: BQ76952 , Hi
The customer bought BQ769142, BQ76952 and BQ7695202. They use BQ769142 and BQ7695202 used a logic analyzer to analyze the signal of I2C BUS, and found these two ICs. Always reply NAK…
Part Number: BQ769142 Other Parts Discussed in Thread: BQ76907 Tool/software: Hi,
Do we have any solution for VRFB?
Its voltage is from 1V~1.2V.
Thanks.
Part Number: BQ769142 Tool/software: Dear support,
i am considering to use BQ769142 in my design and i have a simple question.
I want to use it just to read information on I2C bus and to perform cell balancing, i don't want to use it to cut current…
Part Number: BQ769142 Tool/software: Situation: bq769142 with a STM host processor for a drone battery
Problem: I would like to choose between 2 modes for the BMS protections. 1. Ground: all protections (and FET control) turned on 2. Air: no protections…
Part Number: BQ769142 If REGIN and BREG pins are connected to the ground, then is it possible that there will be a short circuit upon powering BAT+ and BAT- (naming based on reference design)? Because in my circuit when I supply 30V from the power supply…
Part Number: BQ769142 Tool/software: Hi Experts,
Good day!
Could you please share more information regarding the maximum current gate driver of BQ769142?
Thank you in advance.
Regards,
Jonathan
Part Number: BQ769142 Hi Team,
Have a good day! My customer meets a technical issue about BQ769142. The project is 48V BMS in E-Bike.
When we set both MCU and BQ769142 in sleep mode, it happens that the BQ769142 will wake up several times in one minute…