Part Number: BQ769142 Hi
I have two query need your help.
According to the TRM Table 4-6.
Assuming that userA is 1mA, a total of 10.7mah is used
1. After DASTATUS6() subcommand is issued, will there be a difference of + 10 or - 10 between 0…
Part Number: BQ769142 HI Team,
Nice to talk with you! My customer has two questions about BQ769142.
1.When the circuit connection as above: The sampling result is that the first 9 strings have correct values. However, the 10th string is on the VC16…
Part Number: BQ769142 Other Parts Discussed in Thread: EV2400 Our initial design for testing has external header connection for an EV2400 to connect to and read values from the BQ. On powerup we are able to successfully read / configure the BQ. I have…
Part Number: BQ769142 Other Parts Discussed in Thread: BQ76952 Hi TI Expert,
We are planning to build a BMS with 24 Lifepo4 cells in series. BQ769142 supports till14 Cells.
I wanted to know weather BQ769142 can be used in two cascaded configuration…
Part Number: BQ769142
Hi,
Need design review of the attached design.
We are thinking of releasing the board out for FAB this weekend, so any help before that will really help.
Here is the schematic:
AUX_BMS-3.pdf
Here is the layout file…
Part Number: BQ769142 Hi
The customer design with BQ769142, 8 series 60AH batteries are used. The voltage and current scales are both 10.
The log data as below. It is a process from charging 5A to discharging 3A. From the data, it can be seen that…
Part Number: BQ769142 The BQ769142 IC has Stackable (built-in interface) as part of its feature, yet there is no mention on how to stack two ICs for higher cell count. It is not possible using this IC alone? Can I stack only be referring to this How to…
Part Number: BQ769142 Other Parts Discussed in Thread: BQ76952EVM
Dear team,
I've having a problem when trying to use the BQ769142 PREDISCHARGE MODE feature.
A description of how the circuit is configured.
All protection FETs are in use and…
Part Number: BQ769142 Hi Team,
CFETOFF is configured as an AD input pin for detecting external switching signals. How to read its input state, is it 0 or 1? No temperature collection is used.
Regards,
Annie