Hello Star,
No, the BJT's should prevent this from happening. See the schematic I mentioned above for an example ( Figure 5-11. Schematic Diagram FETs ).
Best Regards,
Luis Hernandez Salomon
Part Number: BQ7718 Hi team,
Does BQ7718 support random connection? I notice the abs voltage for each pin is 30V, from this aspect, this device can support that, but considering the secondary protection usually not a recoverable protection, so I am confused…
Part Number: BQ7718 Hi,
Based on the BQ7718 datasheet, the typical supply current is 1uA when cell voltage is 4V.
1) What is the IC supply current if the cell voltage is 3V/2.5V/2V?
2) What is the min IC supply current if cell voltage is 4V?
Please…
Part Number: BQ7718 Other Parts Discussed in Thread: BQ76952EVM , BQ77216 Hi Team,
According to the datasheet, the relationship between VDD and VOUT is shown below.
Then how to design the resistors below in BQ76952EVM if each BQ7718 has different number…
Part Number: BQ76952EVM Other Parts Discussed in Thread: BQ7718 Hello TI forum! My name's Pedro and I'm currently developing my own board using this chip. I noticed the EVM uses a secondary protection system composed by the BQ7718 overvoltage protection…
Part Number: BQ7718 The part we are thinking to use is: BQ771809DPJT.
We want to use this to charge 5 batteries and then switch to using these batteries in series to power a stepper motor. We are making a PCB and would like to know how to do the connections…
Part Number: BQ7718 Other Parts Discussed in Thread: BQ77216 , , BQ77207 Hi,
my customer is looking for a device / solution similar to BQ771824 but with an OVP = 3.8V threshold.
Is there anything we can recommend?
BR Josef
Part Number: BQ7718 Hi Team,
According to datasheet, there is only DPJ package option for BQ771809, but customer prefers DGK package.
Do we have DGK package option for BQ771809 as well?
Regards,