Part Number: BQ79656-Q1 Dear Nancy,
1. as part of our BMS design, we are using BQ79656-Q1, we are facing the problem of BQ79656 doesn't respond to any Messages after the wakeup phase is completed and both TX&RX lines are High state only.
2. Does auto…
Part Number: BQ79656-Q1 Hello,
I am creating a 32S battery monitor with two BQ79656. I have a question about the current sensing in the stacked configuration: do we use the current sense only on the base device, or do both devices need individual…
Part Number: BQ79656-Q1 Hi Team,
Customer is using our BQ79656 and when they download GUI and install but there is no Composer Runtime file.
May I know where we can download Composer Runtime file?
Thanks.
Part Number: BQ79656-Q1 Dears,
We are using BQ79656-Q1 in our Fail safe BMS board design.
Now we are considering 1 00 Micro Ohm current sense resistance for minimum power loss on the board.
we have seen in the data sheet that current sense (16 bit…
Part Number: BQ79656-Q1 Other Parts Discussed in Thread: BQ79616 Hi TI Team,
Currently we are using BQ79656-Q1 IC for our Automotive BMS project. We are using one host microcontroller & single BQ79656-Q1 IC to read cell voltage. In the sample code provide…
Part Number: BQ79656-Q1 Hello,
a colleague of mine has following question:
During the execution of the Voltage Comparison and Cell Balancing FET Diagnostic (executed one after the other, no matter in which order), errors are set in the surrounding…
Part Number: BQ79656-Q1 Hello,
My company has purchased the BQ79656-Q1 IC for the development of an RnD project, and I would like to know if I can have the safety manual of that specific IC, as it is TI Safety Compliant.
Part Number: BQ79656-Q1 Dear Team,
While measuring the current via registers MAIN_CURRENT_HI & MAIN_CURRENT_LO, without connecting any load or charging CURRENT_LO register is showing some random values frequently.
Is there any configuration for…
Part Number: BQ79656-Q1 Other Parts Discussed in Thread: BQ79616 Dears,
we are using BQ79656-Q1 in our BMS design. We have tried to stabilized SPI communications with micro controller and BQ79656-Q1.
Is BQ79656 device has dedicated SPI ports for SPI…
Part Number: BQ79656-Q1 Hi,
I'm working on BMS project, Max battery voltage is 120v, max battery current is 150A and 280Ah battery capacity.
I'm using BQ79656 as battery cell monitor(BMS ic), BQ79630 as battery pack current and protection,
My…