Part Number: BQ79656-Q1 For a BMS based on BQ79656 with similar hardware/circuits like the EVB, the cells insertion (x16 cells) can be one by one or the whole stack 'must' be plugged at the same time?y
We are looking for connectors and we are not sure…
Part Number: BQ79656-Q1 Other Parts Discussed in Thread: BQ79656EVM-021 Hi All,
I'm using BQ79656EVM-021 and BQ79600EVM-030 (Bridge evaluation board)
BQ79656EVM-021 evaluation board is connected with BQ79600EVM-030 on Daisy Chain protocol
I want…
Part Number: BQ79656-Q1 Hello,
I'm looking for the specs of the BQ79656. Alll that's linked to, on both TI's and the distributors' pages, is a 13-page overview that doesn't tell me anything about actually using the thing.
Part Number: BQ79656-Q1 Hello,
we need the input capacitance (Cin) and the acquisition time (t acq) of the Main ADC of BQ79656.
This information is mandatory to select the bandwidth of the input filter of the analog-front end. We don't want to use…
Part Number: BQ79656-Q1 Hello,
I am working on a project where i have to perform ring communication between BQ79652 and BQ79612 ICs. I have connected the COMH of upper device to COML of lower device. But i cant wake up the stack device. I am sending…
Part Number: BQ79656-Q1 Does auto-addressing have to be done before the bq79656 can be put into the Communication Debug Mode?
Can the unlock code (0xA5) be the first message sent to the device after a WAKE signal on the RX line?
To send the unlock…
Part Number: BQ79656-Q1 Other Parts Discussed in Thread: BQ79616-Q1 , BQ79616 /***********************************************************************************************************************
* DISCLAIMER
* This software is supplied by Renesas…
Part Number: BQ79656-Q1 By reading the (full) datasheet, the below topics seem not clear:
What is the circuit for the analog front end of the current measurement? Does it include any instrumentation amplifier?
What is the CMRR for the current measurement…