Paul,
The srec file can be programmed into the device using bqStudio or bqProduction. The other two file formats a special files that contain the commands and data to program the parameters into the flash memory. They are available to use with a custom…
Hi Kurt,
The command need to be send really quickly one right after the other. Also, they need to be sent in little endian format.
For programming the bq78350, you will want to consider our tool bqproduction. You could also use the hex dump functionality…
Part Number: BQ34110 Other Parts Discussed in Thread: BQSTUDIO , EV2400 , BQMTESTER , BQPRODUCTION , BQ34110 Hi,
Once I have created by golden image files using bqStudio, what is the best set-up for programming devices during production?
Would I use…
Our options for programming the srec to the device without using bqStudio or bqProduction are limited. I need to discuss this with our tools team to see what we can offer.
Tim
The bqStudio and bqProduction tools do not run from the command line. I have an applications brief on the bq34z100-G1 website that provides examples of reading and writing registers on the device. It should help with implementing the parameters listed…
Other Parts Discussed in Thread: BQ40Z60 , BQSTUDIO , BQPRODUCTION Hello!
I am creating a 2S1P design with BQ40Z60 close to the reference EMV-Design.
However, i experience voltage drops from ~12V to 8.6V on the ACP-Pin (using BQStudio for reading…
It looks like (from the pictures) you are using an older version of bqProduction. Can you download the latest version from the website and see if that fixes the problem.
www.ti.com/.../BQPRODUCTION ;tisearch=Search-EN-Everything
Hi Srinivas,
bqStudio and bqProduction (used for mass production) are licensed for use by TI customers for evaluation and manufacturing. It is free, there is no fee.
Both are not open source as the intent is to use only with TI products. The license…