Part Number: BQ76952 Other Parts Discussed in Thread: BQ76942 Hi,
I have gone through the datasheet of the bq76942 and bq76952 battery monitor and protection ICs and am considering using them for the BMS that I am developing. I see that the products…
Part Number: BQ34Z100 Other Parts Discussed in Thread: , BQ76952 , BQ76942 , BQ78350-R1A , TIDA-00792 , BQ76930 , BQ76200 , TIDA-010030 , BQ76940 , BQ40Z50 , BQ40Z80 Hi,
I am planning to use the bq34z100, gauging IC along with a non-TI battery monitoring…
Other Parts Discussed in Thread: GPCCHEM I submitted two data files for two different flavors of lead acid batteries and I was wondering as to why I got not response. The tool when I did not provide the files in the format it was looking for emailed back…
Part Number: BQ40Z50-R2 Hello,
I previously successfully completed a learning cycle with a 4s1p version of my pack (we're using Panasonic UF553450Z cells, chem ID 2675). I'm now trying with a full, 4s9p configuration, and am having a problem with getting…
Part Number: BQ34Z100-G1 Other Parts Discussed in Thread: SN74HC164 BQ34Z100-G1 four LEDS configuration as GG file, use external LEDs in I2C communication, but only two LEDS on, the other's are off. 8SP-0035-V0.pdf 8sp-0035.gg.csv
Part Number: BQ40Z60EVM-578 Other Parts Discussed in Thread: BQ40Z60 Dear All,
I am confused.
I was trying to make my own PCB with the BQ40Z60 working but I failed. Because that, I decided to buy the evaluation board, to check if my concept is OK…
Part Number: BQ40Z50 The issue is related to LED display of bq40z50; After a 2C rated discharge , the RSOC decreases to 0%,LED1(one led) is normal flashing light,wait 3-5hours,the led change to two lights on,but the RSOC is still 0%,why?
LED config…
Part Number: BQ27426EVM-738 Other Parts Discussed in Thread: BQ27426 , GPCCHEM , Hey all,
during the manual learning cycle with BQ27426 an error [VOK: Not Clear] is generated.
Conditions:
Charge Setup: Notify when FC-Bit is set
Discharge Setup…
Part Number: BQ34Z100-G1 Other Parts Discussed in Thread: GPCCHEM Please see attched gg , log and srec files.
TrueRC, TrueFCC all drop in value during discharge in low temperature. lowtemp test.rar
TrueRC drops from 10024 to 3062. TrueFCC drops from…