Many thanks Jianzhong,
I will archive those links -
Our board is a custom board based on the Zoom OMAPL138 EVM.
With this we use a virtual machine customised for our hardware which we cross-compile the application on .
This works for the fixed point…
Andreas Dannenberg Yes, these logs differ. This is my do_install()
do_install() {
install -d /data/projects/TI/ti_ws_4/tisdk/build/arago-tmp-external-arm-glibc/work/am62axx_evm_visteon-linux/ti-rtos-firmware/08.02.00.04-r3.0/image/lib/firmware/pdk…
Hideki,
hideki said: A8 <-> DSP communication because it was c6accel, Will there is a bug in the framework?
I am not familiar with the c6accel, but from what I can see this c6accel software development tool is obsolete and not recommended for new…
Hi Kevin,
Are you running Linux on the ARM? My recommendation would be first to start with the DVSDK for DM3730:
http://www.ti.com/tool/linuxdvsdk-dm37x
Besides the Linux board support package for the ARM, this comes with video codecs and "c6accel" that…
Hi,
C674x DSPLIB which can be downloaded from here focus.ti.com/.../sprc900.html .
Once you modify the function you can recompile the library and link it by adding the rebuilt version of this library to $(c6accel_install_dir)/dsp/libs. Adding a new…
Hello,
I am evaluating EZSDK5.03 on TI816xEVM. EZSDK5.03 does not include C6Accel and C6Run (which is included in EZSDK5.02.)
- Can I use C6Accel and C6Run in EZSDK5.03?
If yes, - Should I download manually from below link? http://www.ti.com/tool/c6accel…
Hi Siddharth,
Thanks for the reply.
1) Will TI look into C6accel issue if I have problem with C6accel on DM8168 ?
My concern is that TI might not support C6accel on DM8168.
Is C6accel becoming an obsolete tool ?
Without C6accel tool, what…
I found C6Accel late this afternoon. When I read the wiki, it sounded like it had to be called from the ARM . You're suggesting it's called from the DSP. Or can it be called from either?
-> Yes, It is a tool for an ARM application to invoke…
The C6Accel software product is very likely what you should evaluate as it does support the OMAP-L138 platform, among others.
http://focus.ti.com/docs/toolsw/folders/print/c6accel-dsplibs.html
The C6Accel software incorporates the DSPLIB functionality…
Try using twiddle function included in DSPLib instead of the one from c6accel. Remember about setting the right scaling factor for twiddle generator.
Kind regards
Konrad