Other Parts Discussed in Thread: MSP430G2955 , MSP430G2553 We are considering using the MSP430G2955IRHA40R part with the CAPSENSELIBRARY. I can not find any list of compatible processors with the CAPSENSELIBRARY. (aside from the MSP430G2955 processor's…
Other Parts Discussed in Thread: MSP430FR5989 Hello,
Currently I'm trying to use the Capsenselibrary on a MSP430FR5989. But apparently the library is not yet compatible with this new chip family. Is it worth porting the library myself, or will there soon…
Other Parts Discussed in Thread: MSP430F2013 Hello folks,
I'm trying to use capSenseLibrary for MSP430F2013/ FG4618 Experimenter's Board. But there seems to be a shortage of memory. The error I see is as below:
Error[e104]: Failed to fit all…
I see two different downloads for CAPSENSELIBRARY.
CAPSENSELIBRARY download 1
slaa491
145 files
0.97 MB
CAPSENSELIBRARY download 2
slac489
70 files
562 KB
Why are there two? What are the differences? Which one is more highly recommended…
Part Number: MSP430FR2355 Hello,
I'm working on a product using the MSP430FR2355 due to its smart analog combos. I have the need for adding a capacitive touch button, but need some guidance. I do not believe the part has the captivate peripheral. …
I would recommend looking at the software found here: www.ti.com/.../capsenselibrary
Specifically, for the MSP432, the software is outside of the SimpleLink SDK package and not currently supported. The capTIvate solution is now promoted and supported…
Juliana,
THere is no internal connection between the GPIO and the crystal oscillator pins. Moreover, the crystal pins are not brought out to the boosterpack headers.
Perhaps you can utilize this alternative :
www.ti.com/.../capsenselibrary
…
Hi Olivier,
The CAPSENSELIBRARY is documented here .
Regarding the Port 2 configuration, it is a common practice to set all unused port pins as outputs and driven low. If left as inputs, they can float, causing the internal logic on a port pin to oscillate…
Part Number: MSP-EXP432P401R Tool/software: Code Composer Studio Hello,
I am working with the MSP-EXP432P401R Launchpad. I noticed the sdk comes with driverlib files, are these the same driverlib files for the MSP432 microcontroller found below
dev…
Dear!
I am using the "Pin Oscillator Method" but not CapSenseLibrary but I direct touch the registers. Ok! I will try your suggestions! :) The variable is some material between dthe plates.