Other Parts Discussed in Thread: CC1101 , CC1020 Hi I am trying to get CC1101 and CC1020 to communicate with manchester coding.
When without manchester coding the communication between CC1101 and CC1020 is fine.
But once open manchester coding, it…
Between power on and reset the chip will be in an unknown state and there is a finite possibility that DCLK will be running. On the MCU side you should thus disable the interrupt until you have done a reset of CC1020 (write MAIN = 0x1E followed by 0x1F…
Part Number: CC1020 I have used SmartRf studio for CC1020 to get register settings, in the past and now I am checking them. We have used the CC1020 in production now for more then 15 years (!), I made a spreadsheet to check the register settings and the…
Dear All,
I am facing one strange problem with CC1020 .
I have configure LOCK Register(0x15) with 0x40 means CARRIER_SENSE (RSSI above threshold, active low
I have two board. One is Remote and other is Receiver.
When I send packet from receiver…
Other Parts Discussed in Thread: CC1020 , CC113L , CC1120 , CC110L , CC115L Hi!
I'm developing a CC1020+MSP430 based RF system, capable to communicate with a TNC by means of the AX.25 protocol. I've read this post, too: http://e2e.ti.com/support/wireless_connectivity…
Other Parts Discussed in Thread: CC1020
Hi,
I am facing problem regarding the data transmission of CC1020.
I am configuring CC1020 to transmit data. I can read and write config register.
When I am sending data on DCLK/DIO, I could not see…
Dear Kato Motoki,
Currently TI only has only one package for CC1020, which is the RUZ package, i.e. there are two orderable part numbers: CC1020RUZ and CC1020RUZR. If you look on TI's CC1020 product folder on web ( http://www.ti.com/product/CC1020/samplebuy…
Other Parts Discussed in Thread: CC1020 , CC1120 Hi,
I am trying to send a signal from a CC1120 to a device using a CC1020. The CC1020 is configured to use FSK modulation however the CC1120 only offers 2-FSK or 4-FSK. Is such a communication possible…
TER said: 1) The engineer that knows SmartRF Studio 6 is on vacation this week, I have to check with him next week. 2) This is dependent on your system. If image rejection is important you have to use the algorithm in the datasheet, if it's not, skip…