Part Number: CC1120EM-420-470-RD
I would like to porting driver to STM32 and found that will block on GPIO2 no response after STX command.
I set "CC112X_SETTLING_CFG = 0x00B" and my partversion is 0x23 no run manual calibration.
my initial register…
Part Number: CC1120EM-420-470-RD Other Parts Discussed in Thread: CC1120 I've ported code to Arduino UNO and that can run Tx/Rx test successfully.
I would like to porting firmware to STM32G071RB board and run the same initial register setting value…
Part Number: LAUNCHXL-CC1352P Other Parts Discussed in Thread: CC1352P Hi, TI team,
I am designing a product using CC1352P and wondering if the reference design is the same for different band of 433, 868 and 915 MHz?
I figure if the band is different…
Part Number: CC1101 Other Parts Discussed in Thread: CC110L , SMARTRFTRXEBK , CC1120 Team,
Customer is looking for evaluation card for both CC1101 and CC110L. The goal is to do some evaluation in the following band: Base freq. 867.999 Mhz, channel spacing…
Part Number: CC1120EM-420-470-RD Other Parts Discussed in Thread: CC1120 Hi
I wanted to ask whether there is any way in which I can directly connect a differential input from antenna to cc1120's LNA pins(19 and 20) without using the circuitry involved…
Part Number: CC1110EM868-915-RD Other Parts Discussed in Thread: MSP-EXP430FR5739 This is my first time doing anything with RF whatsoever, so right now I am just trying to check that my components are working.
The specific devices I'm using are:
1…
Other Parts Discussed in Thread: CC-ANTENNA-DK2 , CC1310 , CC1120 Tool/software: TI C/C++ Compiler Dear Sir,
CC1310-1190 launchpad has PCB antenna, which is an 868/915/920 MHz. instead of PCB antenna. I want to use a omnidirectional antenna. which has…
Part Number: CC1120EM-420-470-RD Other Parts Discussed in Thread: CC1120 We have a CC1120 design (433MHz band) on a new product using a helical antenna.
1. Can TI review our design (layout and schematic)? Do you normally do this?
2. Can TI provide…
Part Number: CC1120EM-169-RD Other Parts Discussed in Thread: CC1120 Hey!
I want to operate CC1120 on 145 Mhz. Reference design is available one is for 169 Mhz .However, I'm unable to match the circuit for 145 Mhz.
Can anyone help me with the changes…
Part Number: CC1120EM-169-RD Other Parts Discussed in Thread: CC1120 , CC1310 , WMBUS , CC1125 Good Day
Is it possible to change the frequency form 169 MHz to 868 MHz in the registers of this module? I have requested a 868 MHz module but received the…