Part Number: CC1120EM-169-RD Other Parts Discussed in Thread: CC1120 Hello,
I am interested in employing the CC1120 for a 169MHz telemetry application.
Is the 169MHz band legal for use in the USA by the FCC?
Also, does TI make a product for 27MHz?
Thanks…
Part Number: CC1120EM-420-470-RD We want to try packet communication between cc1120 and cc1020. First of all, the packet format for cc1020 is unknown. I understand that in order to communicate with the packet, we need to know both the primable and sync…
Part Number: CC1120EM-420-470-RD Dear Sir,
I have two CC1120EM-420-470 (DK) daughter cards, and now I have designed a motherboard to connect it.
But i try to find the CC1120EM-420-470 (DK) daughter card information or documents, they are not show the mechanical…
Part Number: CC1120EM-169-RD Other Parts Discussed in Thread: WMBUS , CC1120 , CC1350 , CC1310 HI All,
CC1120 supports 169Mhz RF brand (N-Mode Wireless mBUS).
After downloading "Wireless M-Bus Protocol Software" in https://www.ti.com/tool/WMBUS , and…
Part Number: CC1120EM-420-470-RD
I would like to porting driver to STM32 and found that will block on GPIO2 no response after STX command.
I set "CC112X_SETTLING_CFG = 0x00B" and my partversion is 0x23 no run manual calibration.
my initial…
Part Number: CC1120EM-420-470-RD I've ported code to Arduino UNO and that can run Tx/Rx test successfully.
I would like to porting firmware to STM32G071RB board and run the same initial register setting value as Arduino UNO.
after issue STX command…
Part Number: CC1120EM-420-470-RD Hi
I wanted to ask whether there is any way in which I can directly connect a differential input from antenna to cc1120's LNA pins(19 and 20) without using the circuitry involved to convert single ended input to differential…
Part Number: CC1120EM-868-915-RD Other Parts Discussed in Thread: CC1120 Does cc1120 support interleaving and spread spectrum?If CC1120 confirms that these functions are supported, which registers are involved in configuring these functions?
Hello Nir,
I am closing this thread since this is very old and I assume that this issue has been resolved.
Please create new thread if you are still having trouble.
Regards,
Part Number: CC1120EM-420-470-RD We have a CC1120 design (433MHz band) on a new product using a helical antenna.
1. Can TI review our design (layout and schematic)? Do you normally do this?
2. Can TI provide any recommendations when using a helical antenna…