Part Number: CC1150 For this part to be considered in our design, it is preferable it is RED certified and has the documentation available to prove this. Is CC1150 RED certified and ready?
Part Number: CC1150 Hi, support team
My customer has the questions as follow:
How much Electric field strength on 3m distance is estimated while using 860MHz by max10dbm?
Thanks so much.
Best regards, Yuki
Part Number: CC1150 My customer is mass product the CC1150 and they have to know the cc1150 minimum number for XOSC_Q1 input.
Because of they are going to change the new oscillator that have output a sine wave of minimum 0.4V peak-to-peak amplitude.
…
From the description above I get a feeling that you don't yet have full overview of what CC1150 can and can't do. Please re-read the datasheet.
The CC1150 is a transmitter only, is it a typo that you wrote that you need transmitter/receiver?
The…
Part Number: CC1150 Other Parts Discussed in Thread: CC1100 , CC-DEBUGGER Can the CC Debugger be used with the CC1150? I hooked one up and CC Debugger/RF Studio seems to detect the CC1150, but I get unstable behavior when running the Packet Tx mode.
Part Number: CC1150 Other Parts Discussed in Thread: CC1101 , , CC1352R , CC1310
Dear E2E members,
I was redirected to this forum by TI Customer support. We are looking at possibilities to implement square-root raised cosine (RRC) pulse shaped QPSK transmission…
Part Number: CC1150 Other Parts Discussed in Thread: CC1310 We are planning to use CC1150 at one of the products & may need to increase the RF power output through external power. Can anyone please suggest a low cost external RF amplifier, tested to work…
Part Number: CC1150 Hi,
One of our custom product using CC1150 has some issue with the frequency shifting to 600Khz from 920MHz. The occurance of this issue is very rare and also it occurs with different temperature. Occured once at -17 deg and once at…
Part Number: CC1150 Other Parts Discussed in Thread: CC1101 , CC1310 , CC115L , CC113L I am trying to develop a transmitter and receiver that will send and receive signals via 433mhz.
I want to make sure that whatever I design will end up being able to pass…