Part Number: LAUNCHXL-CC1352P Other Parts Discussed in Thread: CC1352P We are working on adding BLE support to an existing project and the device will assume a peripheral role. Our main issue is that including the BLE stack in our project will increase…
Part Number: CC1352P Other Parts Discussed in Thread: CC2652P , Hi,
I am trying to develop a new system with CC2652P or CC1352P as a replacement according to needs for sub 1GHz, and for the future CC2674P & CC1354P.
If I understood right the RF core are…
Part Number: CC1352P Hi,
I am developing an application for the CC1352 using version 7.40.00.77 of the SimpleLink SDK. One of the modes of the application is a to transmit a CW tone for an unspecified amount of time when it receives a specific serial…
Part Number: CC1352P Hi,
In low battery situation, we need to prevent the SOC crush. Is it possible to get ADC value during transmit. I provide the power curve for your reference.
Part Number: CC2652P Other Parts Discussed in Thread: CC1352P Hi
May I have a question about CC2652P?
I think there is not EVM specific to CC2652P.
So we should use CC1352P EVM for CC2652P develop.
Question:
I think difference of CC2652P and CC1352P is…
Part Number: CC1352P Hi,Ti team,
My collect project base on "simplelink_cc13x2_26x2_sdk_5_20_00_52\examples\rtos\CC1352P_2_LAUNCHXL\ti154stack\collector"
When the collect project run for a while, the ApiMac_mcpsDataReq() func always retrun…
Part Number: CC1352P Hello,
Does TI has an equivalent Duty Cycle Analysis to SWRA396 for the CC1352P? We need it by request of the laboratory currently doing FCC/ISED certification of our product which uses CC1352P as a microcontroller and RF Amplifier…
Part Number: CC1352P Other Parts Discussed in Thread: CC1352R , Hi,
In the application note ( swra629a ), layout of traces between CC1352R and balun is done in the following way, with straight and symmetric traces of RF_N/P.
But for CC1352P, since we need…
Part Number: CC1352P Hi,
If we reboot MCU via the following function:
//#include "sys_ctrl.h"
SysCtrlSystemReset();
RTC will start over from 0. Is there a way to prevent this from happening?
Thanks,
ZL