Part Number: CC2511EMK Hi All,
I am working with the sample applications provided by TI for the CC2511EMK, I am using the "rf modem" example. I don't have the full development board with the kits, I am going to use it with a couple of CC2500's later.…
Make sure both the CC-DEBUGGER and CC2511EMK are connected at the same time, the CC-DEBUGGER LED should be green to indicate that the CC2511EMK is powered and connected. If all other EVM setups are operational then this standalone module could be defective…
Other Parts Discussed in Thread: CC2511 I can't make this combination work. The driver usb_cdc_driver_cc2511.inv doesn't seem to install. When I look at Device Manaqer the CC2511EMK shows as Other Devices CC2511 USB CDC not as a Com port. I have…
Other Parts Discussed in Thread: SIMPLICITI , CC-DEBUGGER , CC2511 , MAX3221 Hi,
The code that I downloaded from the TI website for cc2511EMK rf_modem is using MRFI. Is there a version of rf_modem that is using SimpliciTI?
Thanks!
Other Parts Discussed in Thread: CC2511 Forgive me for this dumb question, I am a newbie.
What is the difference between cc2511emk (i.e., the cc2511 usb dongle) and cc debugger? I think both of them are based on the CC2511 chip, both have USB and Jtag interfaces…
Hey i wanted to output the RSSI value in decibels for each frequency of the entire range of the cc2511emk together with a time stamp for each value into a csv file. Any ideas on how this can be done?
Hi,
Using SmartRF Studio 7 I can adjust settings then export then register values for those settings. Where can I find an example application to build with those register values that I can then burn into flash and power up the CC2511EMK kit with those…
FYI:
Have a look here for info on CC2511EMK FCC:
https://apps.fcc.gov/oetcf/eas/reports/ViewExhibitReport.cfm?mode=Exhibits&RequestTimeout=500&calledFromFrame=N&application_id=660392&fcc_id=ZAT2511USB