Hello all! I
am new to the forum but since I work on a project for CC2520DK, I want
to ask, Where is the PER test info for received packets stored in the memory? And how can I read if?
Many Thanks in advance!
Other Parts Discussed in Thread: Z-STACK
Good day,
I am trying to use the USCI_A1 USART with the Z-Stack on the CC2520DK's EM430F2618. The USCI_A0 USART used by default in Z-Stack's hal_uart.c works fine with my code (using interrupt mode); however,…
Other Parts Discussed in Thread: CC2500 , CC2520 , CC2420 , CC2533 , CC2530 , CC2531 , CC2431 , CC2430 , CC2510 , CC2400 Hi everybody,
I just want to know if there is anyway to exchange between the 2 above mentionned devices, and if yes, how ? I assume the default…
Hi,
I'm starting the SW development of CC2590+CC2520 based design. I'm using the basic software exemples given with CC2520.
The CC2590 PAEN,EN and HGM pins are directly connected to CC2520 GPIO5,4 and 3. In a lot of posts I saw, you said that…
Hi,
I'm using CC2520DK that contain CC2520EM + MSP430F2618EM + SmartRF05EB and 80TK Thermocouple temperature sensor. I'm trying to get the signal from thermocouple and send it to the other node which is connected to PC. I've two questions…
Other Parts Discussed in Thread: CC2420 , MSP430F2618 , CC2511 , MSP430FG4618 , Z-STACK , CC2520 Hi,
Is it possible to use 2420EM with CC2520DK?
Thankyou..
Other Parts Discussed in Thread: MSP430F2618 , CC2520 Hi,
I am currently working with CC2520DK kit.I have a stand-alone application,that activates UART A1 module of MSP4302618.The application writes data to PC and receives data from PC.
The UART A0 of MSP430…
Other Parts Discussed in Thread: CC2520 Hi,
I am working with CC2520DK kit and run into the following problem:
I would like to send non 802.15.4 packets(for e.g. uint8 packet[]={0x11,0x22,0x33,0x44,0x55,0x66,0x77,0x88,0x99};) as a payload data.The length…
Other Parts Discussed in Thread: CC2520 I am working with TI CC2520DK boards and using for debugging TI CC2520DK SW examples.
I found a problem with first read register access to CC2520.
I took as example Reg_read project in IAR workspace.
Activates in…
If you look at the CC2520EMK page on the web ( www.ti.com/.../cc2520emk) you can read the following:
“The CC2520EMK is an ad-on development kit for CC2520DK. The full stand-alone development kit is CC2520DK. The CC2520EMK development kit consists of 2…