Part Number: CC2531EMK Other Parts Discussed in Thread: CC2531 , PACKET-SNIFFER Hi Team,
Customer is trying to connect to a CC2531 on a WIndows 10 machine but encountered a problem which that the Packet Sniffer download does not appear to be a valid ZIP file…
Part Number: CC2531EMK Other Parts Discussed in Thread: CC2540 , CC2511 , CC2531 Hi all.
I am simulating the meandered antenna given in the CC2531EMK reference design. For this, I am following the AN043 "Small size 2.4GHz PCB antenna". The antennas layout…
Part Number: CC2531EMK Other Parts Discussed in Thread: PACKET-SNIFFER
Hello,
I have a query where the captured packets using SmartRF Packet Sniffer where under the APS layer, my APS counter is only either 69 or 174.
Shouldn't it be implemented as a…
Part Number: CC2531EMK Other Parts Discussed in Thread: CC2531 , PACKET-SNIFFER Hello,
I have a CC2531EMK dongle which I would like to use to sniff ZigBee communications.
I tried to follow various examples of how to set the CC2531 up but to no avail.
…
Part Number: CC2531EMK Other Parts Discussed in Thread: CC2531 , , CC2540 was there any real resolution discovered?' Im having the same issue.... cc2531 not showing up at all in windows, but flashes fine etc....... only thing i would like to add is…
Part Number: CC2531EMK Other Parts Discussed in Thread: CC2531 Hi,
Part number which is mentioned in BOM list of CC2531 is not found on webiste.
Even alternate part number is wrong and that is given for Type B while on dongle it is USB Type A.
Please…
Part Number: CC2531EMK Other Parts Discussed in Thread: CC2531 Hi There,
I want to use this module for sniffing 2485 Mhz for development. However the Sniffer Radio config freq is max 2480 MHz meanwhile the chip freq range is 2507 MHz.
What shall I do…
Part Number: CC2531EMK Other Parts Discussed in Thread: CC2531 , CC2530EMK , , PACKET-SNIFFER Hi,
I am using a Windows 10 computer, I have installed SmartRF_Packet_Sniffer2_1.8.0 but when I plug the USB dongle it is not detected by the Packet Sniffer. I can…
Part Number: CC2531EMK Other Parts Discussed in Thread: FLASH-PROGRAMMER , CC2531 , , PACKET-SNIFFER , CC-DEBUGGER When starting SmartRF Packet sniffer software I get a SnifferAgent error: Autostart Warning "No devices are running as expected. Please check…