Part Number: CC2533DK-RF4CE-BA Hi,
We are using the CC2533 in a design coupled with a MSP430 as a target node. And the MSP430 connect to CC2533 via UART .
Is there any sample code or document of target node for reference?
Although obsolete I'd recommend starting with the REMOTI-REFDES and CC2533DK-RF4CE-BA designs. Make sure you have the proper version of IAR EW8051 installed.
Regards,
Ryan
Hello Chirag,
Have you referenced the REMOTI v1.4 resources for the CC2531EMK ZrcDongle project? You should also investigate the CC2533DK-RF4CE-BA and CC2650RC.
Regards,
Ryan
hi, Greenja
this is board: http://www.ti.com/tool/cc2533dk-rf4ce-ba cc debugger fail and this makes me uncomfortable. I just have only a board CC-Debugger.
How else can you help me ?
Other Parts Discussed in Thread: CC2533 , REMOTI , TUSB3410 Dear Sir,
We have bought CC2533 RF4CE DK , http://www.ti.com/tool/cc2533dk-rf4ce-ba
Our host is ARM based embedded system, we target to communicate the device via UART interface to achieve the RF4CE…
Other Parts Discussed in Thread: CC2533 , REMOTI Hello there. I bought this KIT : CC2533 RF4CE development kit. ( Here's the link : http://www.ti.com/tool/cc2533dk-rf4ce-ba ) last week, tested all features and stuffs. Everything is worked fine.
I am…
Hi Bikram,
You should get the "http://www.ti.com/tool/cc2533dk-rf4ce-ba" kit.
This kit also has an IR diode in case you want to be backwards compatible with older technologies.
Hi, I have to develop a automated test to programatically verify a Set Top Box's RF4CE functionality
Tests to be performed:
- Pairing
- Simulate key presses from the remote (programmatically) and verifying it from STB end.
Purchased TI's RF4CE development…
Hi TheDarkSide,
Thanks for the response.
Only the CC2533 Basic Development Kit is shown on the 'ti.com/remoti'.
In one of the paragraph found: " the legacy RemoTI-CC2530DK, now replaced by CC2533DK-RF4CE-BA".
1) Is that means the…
The SensorTag does some of the processing of the data before sending it to the phone. For an application like a pedometer it is no problem to do the processing on the CC2541, for more complex applications it may make sense to use an external MCU and use…