Part Number: CC2541EMK Other Parts Discussed in Thread: CC2541 , CC2540 , CC2652R Hi, I started to use CC2541 mini kit (cc 2540 usb dongle + cc2541 keyfob)
I am very beginner in this module. I am not sure if my idea is correct or not.
My application requires…
Part Number: CC2541EMK Other Parts Discussed in Thread: CC2541 Using SmartRF Studio 7 to control CC2541EMK, I am controlling the LNAGAIN. If I change one of the three LNAs to 0dB, is that LNA bypassed or is the gain changed?
thanks
Part Number: CC2541EMK Other Parts Discussed in Thread: CC2541 I am using an CC2541EMK with a SmartRF05 board and using SmartRF Studio 7. I want to measure the TX signal with a VSA, is there a way to turn the frequency hopping off? I don't see any registers…
Part Number: CC2541EMK Hi all:
I have almost searched all page of TI web , but still can not find the schemetic of CC2541EMK , how can i get one.?
tks.
Part Number: CC2541EMK Tool/software: Code Composer Studio 2541 module, P0_2 (make serial port Rx function)
pins occasionally appear fixed output 0.95V voltage, and P0_2 are not controlled by program.
After this situation, the chip do not lose the power…
Part Number: CC2541EMK Other Parts Discussed in Thread: CC2541 Hi,
Currently I am having SMARTRF05 evaluation Kit & CC2541 evaluation board in hand. I would Like to perform RF performance tests of CC2541. Is there any way to configure CC2541EM in to testmode…
Part Number: CC2541EMK Other Parts Discussed in Thread: CC2541 , I am trying to boot the cc2541-em without the smartrf05. I have the VCC, GND, and RST connected.
It doesn't seem to be booting and actually is erasing flash. Which other pins do I need to…
Part Number: CC2541EMK Other Parts Discussed in Thread: CC2541 , Hi, CC2541 experts,
I'm trying to measure the CC2541 TX power level by using CC2540DK and CC2541EMK.
Even CC2541 max TX power is notified as 0dBm, actual max measurement was about -4dBm…
Hi,
I exactly followed the Chato's setup shown in the photo, But CC debugger's LED is not going green. When I connect to Keyfob it shows green. I already have updated the Firmware on debugger. I have checked the cable also. I tried with another cable…