Part Number: CC2564CMSP432BTBLESW Other Parts Discussed in Thread: CC2564C Hello,
I am working with the BDE-BDM209A part containing the CC2564C and MSP432 controllers. I am using the newest Bluetopia stack (v5.1.1.0). Upon initial connection I see no dropped…
Part Number: CC2564CMSP432BTBLESW Hi,
all Bluetooth Low Energy examples from the CC2564CMSP432BTBLESW-v5.1.1.0-Setup.exe release do not link and the following error is shown:
error #10008-D: cannot find file "SS1BTDIS.lib"
For example, the…
Part Number: CC2564CMSP432BTBLESW Other Parts Discussed in Thread: CC2564C , , MSP432E401Y I am currently struggling to find information on how to add TI RTOS support to the CC2564C Dual-Mode Bluetooth stack on MSP432 (CC2564CMSP432BTBLESW). The online documentation…
Part Number: CC2564CMSP432BTBLESW Other Parts Discussed in Thread: CC2564C Are the optional audio codecs such as AAC, MP3, etc, supported by the Bluetopia SDK? If not, which ones are supported/included in the SDK. I didn't see any mention of audio codec…
Part Number: CC2564CMSP432BTBLESW Hello,
When calling GAP_LE_Perform_Scan I am receiving an error code of -512. Looking in the BTErrors.h include file, this does not seem to be a documented return code.
Normally, this function returns successfully for…
Part Number: CC2564CMSP432BTBLESW Hi Experts,
Client has this problem running the iBeaconDemo and SPPDemo sample projects - which are part of the TI CC2564CMSP432BTBLESW development tools. As per their report, the projects seem to compile and flash the…
Hey Tony,
We have finally figured out the issue. Essentially, the device firmware is not actually loaded onto the CCC2564C. This is because a return value was not properly initialized before it was checked in an if statement to download the firmware.…
Part Number: CC2564CMSP432BTBLESW Other Parts Discussed in Thread: CC256XCQFN-EM , BOOST-CCEMADAPTER , CC3200
My setup: CC256XCQFN-EM MSP432P401R launchpad BOOST-CCEMADAPTER CC3200 AudBoost
Code Composer Studio Version: 10.4.0.00006
BT Stack : CC2564CMSP432BTBLESW…
Hi Gokulnath,
1. You should be able to use the SPP_Data_Write to achieve your functionality:
/*! @brief The following function is responsible for Sending Serial Data to
* the specified Serial Connection. The SerialPortID that is passed
* to…
Thanks for the reply & continued in this thread https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1053852/cc2564cmsp432btblesw-hfp-profile-at-commands-control-commands?tisearch=e2e-sitesearch&keymatch=%20user…