Part Number: CC256XM4BTBLESW Other Parts Discussed in Thread: CC2564 Hello,
I have been working on the blutopia stack and the SPPDemo and was wondering if I could be provided the relevant wiki documents for the SPP demo. The link below is the main document…
Part Number: CC256XM4BTBLESW I have downloaded the software stack "CC256x STM32 Bluetopia SDK" but it not includes the HDP profile.
So, can you please provide me the HDP profile example?.
I can't add this right after the HCI_DRIVER_SET_COMM_INFORMATION macro because the BluetoothStackID, which is returned by BSC_Initialize , does not exist. My exception occurs during the execution of BSC_Initialize .
I feel like I am be using an using…
Part Number: CC256XM4BTBLESW Hi,
I am using mentioned stack on DK-TM4C129x. There is no Headset profile/ example already present. Is it possible to create Headset profile using GOEP? Is there any example using GOEP?
Regards,
Chetana Patil
Part Number: CC256XM4BTBLESW Other Parts Discussed in Thread: EK-TM4C123GXL Dears:
We use EK-TM4C123GXL launch Pad to test CC256X with software CC256x M4 Bluetopia SDKv1.2 R2.
We refer to below link:
processors.wiki.ti.com/.../CC256x_TI_Bluetooth_Sta…
Part Number: CC256XM4BTBLESW Other Parts Discussed in Thread: EK-TM4C123GXL , , BOOST-CC2564MODA Can someone confirm if the combination of these three items (CC256XM4BTBLESW, EK-TM4C123GXL and BOOST-CC2564MODA) are software and hardware compatible?
All of…
Part Number: CC256XM4BTBLESW I work with the SPPDemo.
I send to SPPDemo:
client
Inquiry
pair 1 1
open 1 1
Then the port open needs 100 ms to connect.
When I reset the device, and send
Inquiry
open 1 1
the Open needs 3000 ms
The System have Lost the…
Hi Kobi, can you confirm you use also the library sources from CC256XM4BTBLESW-v1.2-R2 packages? Downloaded from https://www.ti.com/tool/TIBLUETOOTHSTACK-SDK for TM4C platforms. Is it possible to provide us with your sorces? Best regards, Tobias
Jean, The complete clickwrap license agreement is included in the installer (.exe) file for the SDK that is downloaded from ti.com and it is not on the download page. This is how all the SW licenses are delivered. The installer will ask the user to agree…