Dong,
Dong Won Lee said: is there any rule that "A3DP Multiroom isn't working when spp is connected" in Ti Bluetopia Stack?
The A3DPMultiRoomDemo application is only designed to work in the 1 source & 2 sink (one master, one slave) use-case…
Part Number: CC2564 Other Parts Discussed in Thread: CC256XMSPBTBLESW Hi,
I'm testing A3DP & SPP, but this seems to be a problem only for A3DP.
I have implemented an A3DP SNK board and are in the process of streaming music with my smartphone.
To…
Hi Yunoos,
It looks like these errors are caused because of output format (legacy COFF v/s eabi ELF) mismatch between project and libraries. The latest compiler in the CCS7 does not support the legacy COFF mode that the CC256XMSPBTBLESW ccs projects use…
Other Parts Discussed in Thread: CC256XMSPBTBLESW , MSP430F5438A , MSP430F5529 Hi All,
I am looking to implement an MSP430 based Bluetooth host module. I have been investigating the TI library http://www.ti.com/tool/cc256xmspbtblesw . However, it looks like…
Hello Caleb,
Maybe you are suggesting using another UART module, such as UCA1, I think.
I have developed the Bluetooth project by using 'stack code' ( www.ti.com/.../cc256xmspbtblesw)
I was wondering if I can fix the direction of UART pin in…
Hi All,
I am looking to implement an MSP430 based Bluetooth host module. I have been investigating the TI library http://www.ti.com/tool/cc256xmspbtblesw . However, it looks like this library only supports the Bluetooth device end. I am wondering if there…
Hello Anna,
Have you checked the Bluetooth stack for MSP430F5529 support? This is included with the stack, no porting necessary. www.ti.com/.../CC256XMSPBTBLESW
Also, their is a pinout difference between the two devices. You would have to see what…
Hi Sooraj,
For the Stack Init Failed: -4 error, you might want to verify the below items.
- UART connections are configured correctly. Please refer to the CC256XMSPBTBLESW Sample applications for reference.
- The voltage supply to powering up the module…