Part Number: CC2591 Other Parts Discussed in Thread: CC2400 , CC2592 Hi! I am using a Ubertooth one, which has a CC2400 and a CC2591 frontend. The question is, how can I get the actual output power of the CC2591? I have checked the CC2591 datasheet but it…
Other Parts Discussed in Thread: CC2591 , CC2530 , Z-STACK Hi All,
I'd like to program CC2530+CC2591 for personal use: make it listen to a CC2530 GPIO PIN and expose it as a "switch" through Zigbee. Simple, huh? Not for a novice like me.
I…
Part Number: CC2591
RF: Zigbee
Power: 20dbm
Question: After a month of use, the transmission distance becomes closer, 150 meters => 20 meters
Referring to our test result ,we can confirm that there are some problems with the chip "cc2591" . but…
Part Number: CC2530-CC2591EM-RD Other Parts Discussed in Thread: CC2531 , Z-STACK , CC2591 , CC2530 Hi, I am using CC2531 as Zigbee Coordinator Device (ZCD) with Z-Stack_Home_1.2 firmware, CC2530_CC2591 as Zigbee Router Device (ZRD), CC2530…
Part Number: CC2530 Other Parts Discussed in Thread: CC2591 , , CC2531 , RF-RANGE-ESTIMATOR Hi,
I am using Zstack V2.62 and have a cc2591 connected to a cc2530 micro
The connections on the cc2591 are
PAEN to P1_3 on the micro
EN to P1_2 on the…
Part Number: CC2591 Other Parts Discussed in Thread: CC2592 What are the RF parameters of the LNA amplifier in low gain mode.
NF
Ip3
1DBCP?
(in the data sheet only the high gain mode are speceified)
Part Number: CC2541 Other Parts Discussed in Thread: CC2591 , CC2592 Tool/software: TI C/C++ Compiler I am using cc2541+cc2591. I am using these configuration
P0SEL = 0; // Configure Port 0 as GPIO P1SEL = 0; // Configure Port 1 as GPIO P2SEL = 0; // Configure…
Part Number: CC2530 Other Parts Discussed in Thread: CC2591 , , Z-STACK
I am using CC2530+CC2591 for Zigbee 2.0 profile. How easy is to move 2.0 to 3.0 , with keeping same chipset ?
#cc2530 #cc2591