Part Number: CC2650DK Hello,
I am using this board to communicate with a BLE sensor and I would like to know if the BLE power can be changedand if yes how can I do that. Reason is that I want to try to reduce the power so that other sensors near by do…
Part Number: CC2650DK Tool/software: Code Composer Studio Hi,
How to download Project Zero for the CC2650 LaunchPad (modified by another program) using CCS v7?
Thanks
Part Number: CC2650 Tool/software: Linux Hi,
I tried using CCSV6 for programming CC2650DK-7ID. I don't get my device verified while creating my project. This is the message shown.
[Start] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile…
Part Number: CC2650DK Hello,
I'm working on multirole project on stack ble_sdk_2_02_01_18 and tirtos_cc13xx_cc26xx_2_20_01_08 cc2650 DK custom made sensortag devices.
I need to connect the sensortag devices to an android or ios phone to transfer my sensor…
Part Number: CC2650DK Hi,
I am using the document (swra446.pdf) that explains setting up environment to flash and debug apps on cc2650DK using Eclipse+GDB. Application is the simplest blink example.
Now, I've managed to build .bin file, but when I try…
Part Number: CC2650DK Hi,
i'm having trouble implementing I2C to get sensor readings from a BMP280 sensor via I2C. I used the files board-i2c.c, board-i2c.h, bmp-280-sensor.c, bmp-280-sensor.h and the necessary files.
I saw from this question that…
Part Number: CC2650DK Hi,
I would like to ask if this development kit can be used to do OTA without any external devices (Flash). The information that I have found is based on the CC2538 chip but not any literature about how to implement it on the CC2650…
Part Number: CC2650DK Hi all,
Just starting to develop a IEEE mac layer and ran into this issue...
I successfully send "Radio Setup Command" (CMD_RADIO_SETUP - 0x0802) and get CMDSTA_Done (0x01) and subsequently DONE_OK (0x0400) indication that…
Part Number: CC2650DK Good day. I am trying to figure out how to load contiki programs (demos provided by contiki) to the SRF06 + CC2650 platform and for some reason i am stuck when trying to use the .upload make target following the steps found in the…
Part Number: CC2650DK Dear All,
I am complete newbie to CC 2650 . I have purchased CC 2650DK . I have try to run the sample from ZStack home automation, but the 2 CC2650 module is not connected, the status in LCD always Ezmode : timeout for both module
do…