Other Parts Discussed in Thread: MSP-EXP430FR5739 , MSP430F5310 All,
I have two sets of hardware.
A.) The CC3000EM with the MSP-EXP430FR5739.
B.) Our custom PCB with the CC3000 controlled by an Atmel AVR.
I am trying to get up to speed on as fast as possible…
Hi,
The "Errata to TI SimpleLink™ CC3000 Module" dated May 2013 contains the following SW errata relating to v1.11:
2.1 "Connection process will not start for APs with RSSI lower than –75dBm."
Is there a fix for this in…
vivekanand goud j said: i need source code for interfacing cc3000 booster pack with msp430g2553
You can find it in software section of cc3000 product page.
http://www.ti.com/tool/cc3000-sw
http://www.ti.com/tool/cc3000-sdks
I downloaded "SmartConfigJavaApplet-1_1-windows-installer" and "CC3xxxHomeAutomation_AndroidApp-1_11-windows-installer" from http://www.ti.com/tool/cc3000-sw and can't open the file. When I double-clicked them, a pop-up window…
Not sure I understand your situation fully but TivaWare 2.1 has CC3000 examples on both Tiva LaunchPads. Including the patch_programmer that updates the CC3000 firmware.
C:\ti\TivaWare_C_Series-2.1.0.12573\examples\boards\ek-tm4c123gxl-boost-cc3000\…
uma pv said: It is not clear in the data sheet..
Which datasheet are you looking at?
Give the link!
uma pv said: I am using MSP430FR5739 + cc3000 experiment board
http://www.ti.com/product/MSP430FR5739#desKit does not list a "MSP430FR5739 + cc3000 experiment…
Hello Deep,
The booster pack have to be designed as per the Booster Pack Header which is kept same between the LaunchPads. The CC110L is primarily for the MSP430 LaunchPad. You may have to check for (a) pin compatibility between the Booster Pack and…
Other Parts Discussed in Thread: EK-TM4C1294XL , SW-TM4C Hello,
I have some question but my english is not well.
I got an EK-TM4C1294XL and a CC3000 Booster Pack,
then, download the SW-TM4C: TivaWare for C Series software. (http://www.ti.com/tool/sw-tm4c…
tim deleo said:
THATS FOR THE 129 I'M USING THE 123
Yes, I know. I also have Tivaware package for Tiva Launchpad TM4C123 and it does not have the CC3000 example program. TI made the Tivaware Packages for specific Tiva kits and some examples are included…
Hi Sean,
Sorry, but no, you can't do that.
CC3100 is not just a SW\FW update, it is a totally new device with many improvements on top of CC3000. Different chip requiring different schematics and layout.
Thanks, Alon