Part Number: CC3200 Having issue in connecting to Dropbox for OTA. Facing CDN error while trying to connect by presigned url. I would like to have more information on whether the issue is with TI or I need to follow up with dropbox. Below is my device…
Part Number: CC3200 Hi Team,
I want to confirm if there is any small package of CC3200 will be pushed such as DYY, DDF, DDC... And could you share the small package information and RTM time if we have. Thanks.
Best Regards,
Ryker
Part Number: CC3200 Other Parts Discussed in Thread: BOOSTXL-SHARP128 Hello,
I am trying to use an SD card to load bmp images onto the CC3200 Microcontroller board. The breakout board that I am using for this is an AdaFruit! SSD1351, which is an OLED…
Part Number: CC3200 Hello. When the CC3200 is acting as a Wi-Fi station. If the the simplelink device successfully connects to a desired access point but fails to find a DHCP server, then is there a possibility that it will assign itself a link local…
Part Number: CC3200 Other Parts Discussed in Thread: SYSCONFIG Hi team,
I have read https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wi-fi---internal/f/wi-fi---internal-forum/1233489/cc3220moda-wifi-at-command?tisearch=e2e-sitesearch&keymatch…
you can't delete it, but you should be able to re-write it without a token (it was supposed to be created with "public-write" flags that enables overwriting it (note that we use a "downgrade protection" mechanism so you can only use a newer SP - that…
eventually, IT guy turn off wifi 6, make only wifi 4 available, and do some strange setting, which they don't understand why they make it works, now cc3200 can access server via 9120AX.
thanks.