Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: CC3200SDK , UNIFLASH Hi team,
CCS:8.3.0
SDK:1.5.0,CC3200SDK_1.5.0\cc3200-sdk\example\p2p
Mobile phone model: Huawei Mate60
The program stopped in this while, the routine has not been changed…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: CC3200 , UNIFLASH What would be the best way to reset the target processor on a CC3200 Launchpad without reprogramming the flash ?
I've installed the latest Uniflash (8.5.0) and it seems like…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: UNIFLASH , CC3200 , , CC3100 Hi there,
I've only seen this issue on E2E a couple times, with no actual resolution.
In attempting to connect to the CC3200 using UniFlash (3.4.1), I am getting…
Part Number: CC3200-LAUNCHXL-RD I have a 3200 launchpad and cannot provision it.
I can see the wifi AP.
I can see the device in DEVICES.
I can see and am connected to the Launchpad "mysimplelink xxxxxx
When i try to provision it keeps telling me…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: CC3200 , CC3200SDK I am attempting to setup the CC3200 Launchpad on my second laptop and unfortunately I am getting driver problems. More specifically "Windows cannot load the device driver for…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: UNIFLASH , CC3200 Hi,
working with CCS 6.1.0 SDK1.1.0, in debug mode it works perfectly.
After I close CCS, plug off and then plugin USB, it does not work.
Disconnected jumper SO2 but it does…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: CC3200 , UNIFLASH Hi,
I am using CC3200 Launchpad, SDK1.1.0 and CCS6.1.0
No problem to develop software and debug.
Now I would like to make it work in release way.
First, I expected that if i…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: CC3200
I have implemented continuous ping pong uDMA in UART with wireless transmission in CC3200 but I am missing data: shown in image below, new data is not written into the buffer and thus…
If a breakpoint is placed in recv() function, both the task works perfectly fine. The same said issue is there, if the same code is executed without any breakpoints. Can you help this?