Part Number: CC3220R Other Parts Discussed in Thread: CC3120 , CC3220SF
Hello, We need to use SST26VF016BT-80E/SN as the external FLASH memory for CC3220R/S. Looking at the "Using Serial Flash on CC3120 and CC3220 SimpleLink Wi-Fi® and Internet-of-Things…
Part Number: CC3220R I have a Motorola Edge 40 Pro phone and if I try to connect to the CC3220's wifi via Android settings, it disconnects almost instantly (Android13). I have always used a Samsung Tab 7 and I never had any problems until I updated the…
Part Number: CC3220R Hello everyone,
I will be designing a small datalogger with very basic functionalities and WiFi and Bluetooth connectivity for a hospital. The only external hardware I will use is an ADS1148IRHBR for sensor measurements, an LCD screen…
Part Number: CC3220R 如图所示,SDK使用的版本为5.30.0.08版本,连接MQTT服务器时出现错误码-2005,请问这个错误码代表的是什么意思?我该如何修改我的工程?
1.The routine uses the MQTT Client.
2.Ti routine I have tried, the same parameters can be connected
3.This version is not easy to adjust, I was taking over…
Part Number: CC3220R Hi team,
Here's an issue from the customer may need your help:
Projects developed based on CC3220R experienced a chip-out firmware issue during the test phase. This can be seen in the case of an occasional power-up when the serial…
Part Number: CC3220R Hi,
Trying to get an application to be always connected by configuring the power module in common.sysfig as follows
and then enabling the policy and going into sleep.
After the sleep wakeup, I check the return from PRCMLPDSWakeupCauesGet…
Part Number: CC3220R Hi,
Is the problem from this old post fixed yet in the SDK? We still have this problem on our firmware. It is a very critical problem.
e2e.ti.com/.../cc3220r-character-in-ssid-or-password-not-supported
Thanks in advance
Part Number: CC3220R Other Parts Discussed in Thread: CC3200 Hello,
Im using a WDT in my application code, and its initialized as shown below
Watchdog_Params params;
Watchdog_init ();
Watchdog_Params_init (¶ms);
params. callbackFxn = wat…
Part Number: CC3220R Hi team,
My customer is trying to use WIFI Direct mode connecting multiple P2P devices (CC3220) to a PC/laptop (P2P mode), note that they got STA working with a router, are now also trying to get P2P working without need of a router…