Part Number: CC3220S-LAUNCHXL Other Parts Discussed in Thread: CC3220S , SYSCONFIG I have been been using CCS V12.2.0.00009 with TIRTOS7, TICLANG and the simplelink_cc13xx_cc26xx_sdk_7_10_02_23 SDK successfully for some time.
I downloaded simplelink_cc32xx_sdk_7_10_00_13…
Part Number: CC3220S-LAUNCHXL Other Parts Discussed in Thread: ENERGIA Hello Team,
I added a Energia Sketch as shown below:
Building the project worked without error.
Afer pressing the Run button I got below error:
The project folder looks…
Part Number: CC3220S-LAUNCHXL Other Parts Discussed in Thread: CC3220S , SYSCONFIG Dear TI Engineers,
I own a CC3220S Launchpad.
I want to develop a Wi-Fi station on it and connect it to other Wi-Fi Access Point through Wi-Fi Protected Setup and Button…
Part Number: CC3220S-LAUNCHXL
Hello,
Currently I am working on Smart Door lock project and the firmware is edited for our similar kind of application , I have added AWS MQTT for server communication. Now i need to enable the Power Policy.
The power…
Part Number: CC3220S-LAUNCHXL Hello,
I want to use CC3220 in transceiver (promiscuous) mode to communicate with each other. Means, I want to transfer custom data without wiFi connection. I have the following question.
1. What is the PHY modulation…
Hi Moshe,
Could you inform me on which board revision of the CC3220S-LAUNCHXL you are using? Can you also list the jumpers you are repositioning when switching from 5V to 3.3V?
Part Number: CC3220S-LAUNCHXL Hi Support,
Below are the Sequence of steps that are followed
When the device is in Provisioning mode, i.e., in AP+SC mode, I have sent a http post request that contains the country code to be set. So, when I get the…
Part Number: CC3220S-LAUNCHXL I followed the directions to the http server demo. Once I flash the firmware on to the development board and reset the processor I am getting a 404 error on the web server and the serial port is not reporting any data to…
Part Number: CC3220S-LAUNCHXL Other Parts Discussed in Thread: CC3220S , UNIFLASH We have designed CC3220S custom board for our project. The issue is some MCUs are detecting while we check from the UNIFLASH tool. We have purchased ICs from the Digi key…
Part Number: CC3220S-LAUNCHXL Other Parts Discussed in Thread: CC3220S , UNIFLASH Hello,
I want to perform RF test (sensitivity and Tx power in non ignaling - no connexion with a another device) with the CC3220S Launchpad
I'm trying to use Radiotool…