Hi Pete,
For EAP connection is supported TLS 1.0 only. There is not way how this can be changed from your side. TI have decided that they will not add support for TLS 1.2 for EAP at CC32xx and CC31xx devices (including latest CC3235 generation). It is…
Hi Venu,
Yes, I understood. Maybe there can be way how get to work CC3235 with two layer board, but re-design your board to four layer is a preferable way.
btw ... Do you want to use EAP (WPA2-Enterprise) WiFi security at CC3235?
Jan
Hi,
sFlash is SPI chip connected to FLASH_SPI_x pins of CC32xx QFN chip. Without sFlash CC32xx cannot operate. sFlash is used as storage for execution image, patches for NWP - called ServicaPack, configuration files for NWP, files for internal http server…
Hi,
Has you update Service Pack together with SDK?
I am not able to say what is going on without debugging real code. Maybe if you capture NWP log from your AP and STAs at same moment, maybe there can be some clue. How to capture NWP log you can find…
Hi,
That SDK and ServicePack should be fine. For WPA3 there is no need to set something else than SL_WLAN_SEC_TYPE_WPA3.
I never tested WPA3 with CC3235. But I have validated that WPA3 works with CC3220 fine. I would not expect any difference at WPA3…
Please refer to the programmer's guide which includes features that were added through service packs.
- WPA3 is supported.
- FIPS is still at 140-2
- 802,11 ac/ax are not supported by CC3235 (11ax is supported by CC3301 )
- Some Features from 11k and…
Part Number: CC3235S Other Parts Discussed in Thread: UNIFLASH Hi All,
I have designed a custom board based on CC3235S (replicate the design, provided in the datasheet). It powers up properly, and I can see the 1.9 and 1.2 volts on the DCDC ANA and DIG…
Part Number: CC3235S Other Parts Discussed in Thread: UNIFLASH , Hi all,
I have designed a custom board for a CC3235S processor, replicating the schematic provided in the datasheet with identical component values. I am unable to connect to the board through…
Hi,
IPv6 is not supported at AP mode for CC3120. IPv6 is supported only at STA (client mode). This is same for all CC31xx and CC32xx device (e.g. CC3120, CC3220, CC3135, CC3235). At AP mode is IPv4 supported only.
CC31xx devices does not support AT commands…