Part Number: CC3235MODS Other Parts Discussed in Thread: CC3235S , Hi,
We are under review to design the product using CC3235MODS module.
Can the CC3235MODS module run AT Command directly using Uart from an external MCU without programming?
Or can the…
Part Number: CC3235MODSF Other Parts Discussed in Thread: CC3235MODS
Hello,
I'm currently working on a connected tool project, to communicate via wifi, the product is equipped with the CC3235MODS or CC3235MODSF wifi module depending on availability.…
Hi Chris,
Apologies for the misunderstanding of the question. As Jan mentioned the need for shielding depends on your product design, but it is not always necessary to put a "gasket" on the device itself like the CC323xMOD. The CC3235MOD has…
Part Number: CC3235MODS Other Parts Discussed in Thread: CC3235SF , CC3235MODASF , CC3235MODAS Dear all
There seem to be serious availability issue with most of the CC3235 modules. When considering using a HF-microcontroller (e.g. CC3235SF12RGKR) to build…
Part Number: CC3235MODS Other Parts Discussed in Thread: , UNIFLASH , CC3235S , CC3235SF Hi experts,
We are using to CC3235MODSF. however, due to delivery issue, I would like to use it compatible with CC3235MODS.
is it possible to use it compatible wit…
Part Number: CC3235MODS Other Parts Discussed in Thread: CC3235S I have a roaming portable device setup as HTTP server that gets in to and out of range. I would like to know if there is a way to send a GET message to server IP port 5000 when ever the device…
Part Number: CC3235MODS Hi team,
Here's the request from the customer:
The initial power-on Reset waveform cannot meet the requirements of the specification. Does it need to be processed by the customer (such as connecting a large capacitor in parallel…
The is 30 entries.
You can filter the results to include only those with RSSI above a certain threshold or only scan specific channels:
_i16 Status;
SlWlanScanParamCommand_t ScanParamConfig;
ScanParamConfig.RssiThershold = -70;
ScanParamConfig.ChannelsMask…
Part Number: CC3235MODS Other Parts Discussed in Thread: SYSCONFIG Hi,
Thanks to this forum, I end up development phase of CC3235MODS project.
When we implemented these modules in the target factory and did test running, We found that
we need to improve…