I've been using the PPWC program for over a year on a project. I've just recently upgraded to version 1.3.0.36447 and created a new custom project. My quandary, when I select the Custom design option for the Hardware platform, I do not get the Audio Device…
Hello Experts,
I'm trying to use PPWC to customized ADC3101's miniDSP.
However, the memory size seem's too small. Error message : " Audio Device I2C Configuration too large! "
Is there any possibility to overcome this problem?
B.R…
Hi Experts,
We need a way to dynamic change Master's logic channel and latency dynamically, and already search E2E.
It seems we have to re-download master's firmware, is it still correct now or new 85xx firmware will be released?
Another question…
Other Parts Discussed in Thread: TLV320AIC3204 , TAS5708 , TAS5713 , TLV320AIC3254 , TAS5710
Hi all,
there is now an update available for the PurePath Wireless Configurator software. Enhancements in PPWC version
1.0.1 includes support for new…
Hi Flor,
the immediate point I can think of is that you are not pulling the "Digital audio input valid" pin low. If this is the case, you should see the audio clocks on the slave device but no activity on the audio IO. The "digital audio input valid…
Part Number: CC8530 Other Parts Discussed in Thread: CC8530 Hi
I've read the datasheet for cc8530 and the user manual too, but I still have a couple of questions that I hope someone can answer. I'm looking at using the cc8530 to connect both audio and…
Hello I had a quick question on the read/write endurance of the SPI on the CC85XX
..Lets just say I didn't have an interrupt line to a host controller from a CC85XX, and because of that had to poll the SPI status word diligently in order to see if…
Other Parts Discussed in Thread: PUREPATH-WL-CFG Hi All,
When there is no audio input to CC85xx Master,(i.e. audio silence)
Is it possible to autonomously stop the communication between the slave?
Do you need an external control?
Regards…
Other Parts Discussed in Thread: CC8531 , PUREPATH-WL-CFG CC85XXDK-HEADSET said: "However firmware with USB support is not yet available upon the release of this kit." CC8531 said: "Built-in audio protocol -CD quality uncompressed audio -Excellent robustness…
Other Parts Discussed in Thread: CC8530 Hi,
i noticed that the 8520 has the bandwidth to send 5 Mbits/sec. Is there a way to utilize the full bandwidth? For example by defining more than 2 logical channels.
thanks
dan