Part Number: CCSTUDIO-MSP Hello, I am having the same issue as everyone on this thread. Could you please share your solution with me?
I'm also running Windows 11
Thanks
Part Number: CCSTUDIO-MSP Team,
A customer of mine is using CCS 11.2. But they now have an issue on 4 PCs: after the program was running for the first time, they terminate the debug session, recompile the program, it gets reloaded, but then the play/stop…
Part Number: CCSTUDIO-MSP Hi all.
I'm running ccs version 10.4.0.00006 for ubuntu
This was working one day then not. I can't set breakpoints in linked C source files - the main file is ok.
In the llinked file, the right click in the left hand indexed…
Part Number: CCSTUDIO-MSP
Hi team,
My customer have Msp430f1232 chip and program it with code composer with BSL bootloader. He want to know there is a method to read out code from MSP430F1232 and format in hex file in CCS.
He bought a MSP430G2 lunch…
Part Number: CCSTUDIO-MSP Hi team,
When running the CCS 11.0.00012 installer, the MSP430 or MSP432 components cannot be installed and an error is reported, then exit. The error message is as follows:
CCS_ERROR: Unable to install repotype executable D:…
Part Number: CCSTUDIO-MSP Hi, My customer wants to modify text editor in CCS, so that "Tab" is not displayed as "space" x n characters. There is "Insert spaces for tabs" Option in Text Editors preference window and its default setting…
Part Number: CCSTUDIO-MSP Hi Experts, A customer would like to use an OpenMSP430 device. With this case, the license for MSP430 is applicable? They need to confirm about the license condition in the"MSP430_RTS_20.2.0.LTS_manifest.html" and "MSP430_RTS_20_2_0_LTS_561e8470…
Part Number: CCSTUDIO-MSP I am unable to download the installation for the selected components MSP 430 and C2000. I have attached the installation logs.
ccs_install_10.4.0.00006.log
Log started 08/23/2021 at 13:48:15
Preferred installation…
Part Number: CCSTUDIO-MSP
By default, CCS will detect the JTAG interface automatically based on the device and the debugger. However, you may want to manually change the interface type to 2-wire SBW or 4-wire JTAG. Currently, CCS does not allow you to…
Part Number: CCSTUDIO-MSP There is a problem running ccs.
Set workspace and press Next to turn off ccs without error message. If I delete the workspace's .metadata and run it again, the same result. The contents of workspace-.metadata-.log are as follows…