Part Number: CD40109B-Q1 Hello E2E Experts,
Good day.
CD40109BQNSRQ1:
We are trying to protect this chip for automotive applications. I can't find how much voltage the inputs can withstand on the datasheet. It states that VCC can Exceed VDD, but not by…
Part Number: CD40109B-Q1 We are trying to protect this chip for automotive application. I can't find how much voltage the inputs can withstand on the datasheet. It states that VCC can Exceed VDD, but not by how much. It also states the input signals can…
Part Number: CD40109B-Q1 Other Parts Discussed in Thread: UCC27517A-Q1 Hi,
We have a requirement of level translation from 3.3V to 12V logic levels. Please let me know whether the part# CD40109B-Q1 is suitable for this purpose? If this can be used, please…
Part Number: CD40109B-Q1 Team,
For the device, my question is showing as below.
1. If there is unused ch, what is the suggested connection? GND/Vcc/floating?
2. Do I need to set default value on input side?
Roy
Part Number: SN74AHCT1G126-Q1 Other Parts Discussed in Thread: UCC27517A-Q1 , CD40109B-Q1 Hi team,
I have a customer that wants to use the SN74AHCT1G126-Q1 for their design to move 3.3V logic to 6.5V, however the part says the max is 7.0V and they feel…
Part Number: SN7404 Other Parts Discussed in Thread: UCC27517 , TXH0137D , CD40109B , TXH0137D-Q1 , UCC27424 Hi,
I am looking for a voltage level conversion chip or buffer.
I need to convert my signal voltage from 3.3V to 15V.
SN7404D seems not to be the right…
Part Number: CD40109B-Q1 Hi team,
Can CD40109B-Q1 achieve 5V to 15V voltage level shift and 15V to 5V voltage level shift unidirectionally? The max. frequency of input is about 20kHz . How to set up the VCC, VDD and EN pin?
Is it right configuration for…
Part Number: CD40109B-Q1 Other Parts Discussed in Thread: P82B96 , Hi Team,
My customer is asking if we have level shifter solution support 18V~6.5V to 1.8V GPIO application. Is CD40109B-Q1 the most proper solution to fit in? Also found another one P82B96…
Part Number: CD40109B-Q1 Other Parts Discussed in Thread: SN74LS07 Hi,
I need to design a circuit wherein +3.3 v pulses coming from FPGA have to be converted to +20+/-5v signal(LOGIC 1: between +15v to +25v and logic 0 : 0v ).CD40109B-Q1 seems to be…
Part Number: CD40109B Other Parts Discussed in Thread: UCC44273 , UCC27517 , TXH0137D-Q1 , CD4504B , TXH0137D ,
This is reg translating a 3.3 V PWM Signal to +15 V levels with approx 5 mA Source & Sink
CD4504 Data Sheet is not guaranteeing this translation…