Part Number: CD4027B Other Parts Discussed in Thread: SN74HC109 , SN74LVC112A , , SN74HCS74
Hello all,
I would like to know if CD4027BE can be used as a direct replacement for CD4027BCN.
I have put together a simple toggle switch circuit based on the…
Part Number: CD4027B Other Parts Discussed in Thread: CD4016B , , TS12A4514 , CD4066B Dear * all,
i changed the input buffer form CD4050B for a CD40106B so i connected
-> button from Pin1 ( CD4016B) to gnd, and added a 100k pull-up to 12V from Pin1 ( CD4016B…
Part Number: CD4027B Other Parts Discussed in Thread: CD4050B , CD40106B Dear *,
I attached my schematic with CD4027B. I have connected toggle button on P2 and when press the button the 14V comes to K1, J1 and through R10 10Ohm C8 100n to CLK1 but the…
Part Number: CD4027B My customer would like to know the exact proper way to tie unused pins on the TI CD4027 JK Flip-Flop.
That is, he is using only one flip-flop in the package. Should J, K, S, R, Clock all be pulled low or should R be pulled high and…
Other Parts Discussed in Thread: CD4027B Hello,
I want to simulate the CD4027B, but i don't have a model .lib or .cir for create the component. It will be created a card with this component and it would be desirable to simulate this function under LTSpice…
Hello,
We are closing this post due to its age.
If you have additional questions, please feel free to start a new thread, and we would be very happy to help!
Best,
Michael
Part Number: CD74AC109 Other Parts Discussed in Thread: CD4027B , , SN74HCS74 , SN74AUP1G80 Dear TI team,
I want to use a master slave JK Flip flop to toggle the output when Clk is generated. A tactile switch will be connected on clk signal to operate it…