Part Number: CD4041UB Other Parts Discussed in Thread: SN74AHCT125 , SN74AHCT04 Hi,
I am also looking at complimentary buffer options to re-drive like the CD4041UB. Are there newer complimentary buffer options? It looks like the CD4041 needs a Vih_min…
Part Number: CD4041UB Hi ,
I want to use CD4041UBPWR ,it is new componnent for me , can you PLS tell my about the relability of the CD4041UBPWR?
Thank you.
Ilan mazuz
Part Number: CD4041UB Hi Ti,
PLS advise if can i drive with IC PN CD4041UBPW (VDD=10v) the optocoupler PN PS8101 at temperature range from -40C to 85C ?
1.when i have 277 ohm near to output driver in series connect to another series resistance of 250…
Part Number: CD4041UB Hi,
in order to gקא more current can i shorts the inputs to the input signal ,then short the outputs to the output signal?
BR,
Ilan
Hi TI expert,
Now I need a buffer to drive a power FET(Low side) which input cap is 2nF cap at high frequency (10MHz) but it needs 400mA CMOS buffer at 12V.
I look at your buffer area.... I only find CD4041UB - CMOS Quad True/Complement Buffer which is…