Part Number: CD4044B-MIL I am looking for guidance on when this SR latch is in the 'forbidden' state with S and R both set to 0 what the logic output is; the data sheet has a note saying this output is dominated by R = 0, but no state table to show the…
Part Number: CD4044B Other Parts Discussed in Thread: CD40109B Hi
We are using CD4044B chips connected to 15Vcc. Therefore, the latched outputs signals(Q1,Q2,Q3 and Q4 of the chips) of the chips will be at 15V. What would be the best solution to translate…
Part Number: CD4044B Other Parts Discussed in Thread: SN74AHC00 , SN74AHC02 Though the recommended operating conditions specified in the datasheet indicates it can work between 3V and 18Volt. But all the parameters in the datasheet seems to be tested based…
Part Number: CD4044B Hi Team, My customer considers to use CD4044B. If he doesn't use Q4, is the following correct? Q4=open, S4=R4=GND(0V) Best Regards, Yaita / Japan disty
I think the easiest way to build this would be to simply combine the comparator with an actual set/reset latch, i.e., CD4043B or CD4044B, or made from two NAND or NOR gates (SN74LVC2G00/SN74LVC2G02).
Part Number: CD4044B In the datasheet of CD4044B the input high voltage is specified for supply voltage of 5V, 10 V and 15V. But we are operating at a supply voltage of 3.3V and I would like to know the Vih for 3.3V supply.
Kindly suggest the solution…
Part Number: CD4044B Hello guy,
Datasheet http://www.ti.com/lit/ds/symlink/cd4044b.pdf page 1 Truth Tables shows S=0, R=0, E=1 Q= the double triangle.
Is this correct?
Part Number: TIDA-00366 Other Parts Discussed in Thread: TLC372 , CD4044B , TLV1701 Dear Team,
In the TIDA-00366 design, overcurrent protection is implemented through comparator circuit.
It is also mentioned that short circuit protection is also incorporated…