Part Number: CD4504B Other Parts Discussed in Thread: SN74LV6T17 , OPA4197 , TXH0137D-Q1
Hi Clemens
Thank you for your prompt answers as always.
While your answer was meticulous and rigorous and I thank you for that ,
if I were to reduce my Source & Sink…
Part Number: CD4504B-EP Other Parts Discussed in Thread: LM293-EP , TLC372-EP , TL331-EP , LM239A-EP Could you please confirm if CD4504BMPWREP can be used for 15V to 3.3V level down shifting.
Under recommended condition , i see 5V as minimum input voltage…
Part Number: CD4504B In CD4504B and CD4504B-EP datasheet, Quiescent current in CMOS-CMOS mode
at Vcc=5V and Vdd=15V is only "0.02 uA" , but at Vcc=5V and (Vdd=5V & 10V) is 1000x higher as "0.02mA" .
Is this currect ?
Part Number: CD4504B Other Parts Discussed in Thread: UCC37324 , UCC27516 , TLC3704
Hello
I am looking for a Low to High ( 3.3 V to 15 V ) Translator with at least 10 mA Source & Sink
capability for Interface between our DSP and IGBT Drivers.
Two /…
Part Number: CD4504B Other Parts Discussed in Thread: CD4093B
Hi,
Background:
I am using the CD4504 to level shift the inputs to my circuit, from the voltage level of a selectable power supply, that can either be 15V, 5V or 3V3, to 3V3 (the inputs will…
Part Number: CD4504B Hello,
As previously posted and deleted , I did ask if F in/out was special or had some other functions and the answer was no.
Now I'm tstill rying to fix an issue with F input/output on CD4505B where F out can't get at 0V when F in…
Part Number: CD4504B-EP Hi Team,
My customer is considering CD4504B-EP and he has following questions, could you kindly help?
1. Can CD4504B-EP convert 15Vin to 5Vout?
2. Is following connection correct to convert 5Vin to 15Vout( High : 15V, Low : 0V )? …
Part Number: CD4504B Hi Sir,
My customer would like design CD4504BPWR.
Would you please review parameters and provide your comment?
Conditions:
Vcc=3.3V
Vdd=7.125V
SELECT=Low (CMOS-CMOS)
What is Vcc spec in datasheet? Only Vdd is available in datasheet…
Part Number: CD4504B Hi,
My customer want to use the case in Vcc=3.3V and Vdd=7.2V. According to related question, I konw Vcc=3.3V can work as well in customer usecase.
But in datasheet of DC4504B, there is no specification of VIL and VIH at Vcc=3.3V…
Part Number: CD4504B Other Parts Discussed in Thread: CD40109B , TMS320F28335 Hi,
I am using f28335 to control an inverter which its drive needs 15V puls for getting ON. I want to use CD4504B for increasing the voltage of DSP PWM from 3.3v to 15v. I have…