Part Number: CDCE6214-Q1EVM Other Parts Discussed in Thread: USB2ANY Hi!
User guide for CDCE6214-Q1EVM explains how to set up the board for external 5V power, but it requires modifying the board and I don't really see the need. What I would like to do…
Part Number: CDCE6214-Q1EVM Other Parts Discussed in Thread: CDCE6214-Q1 Hi Team,
Our customer would like to know the length, width and thickness of CDCE6214-Q1EVM evaluation module. Can you please share this information?
Regards,
Danilo
Part Number: CDCE6214-Q1EVM Hi,
This is an inquiry from our customer. Using TICS.Pro to write the settings to EEPROM with the .tcs file open will result in an error.
Is this operation correct?
There is no problem in writing the .hxt file to the EEPROM…
Part Number: CDCE6214-Q1EVM Other Parts Discussed in Thread: CDCE6214 Hello,
I need to provide a 322.265625 MHz reference clock to an Intel Cyclone 10 GX FPGA for use with an USXGMII interface. This is needed to communicate with a 10GBASE-T PHY from Marvell…
Part Number: CDCE6214-Q1EVM Hi there,
I just started playing around with the eval board and the bias current and load capacitance settings do not make sense to me.
Could somebody provide the datasheet or information on the 25 MHz Xtal used on the eval…
Part Number: CDCE6214-Q1EVM Other Parts Discussed in Thread: USB2ANY Dear team,
I try to connect CDCE6214-Q1EVM to TICSPRO, but failed.
I have follow up with with hardware and jumper setting. And follow section 3.1 of user guide(win7/ update firmware…
Part Number: CDCE6214-Q1EVM Hello Team,
may I kindly ask you for the BOM, especially the PN of the 25MHz crystal, please.
Also, how can I calculate the values of the integrated loop filter to achieve lowest loop bandwidth of 100kHz?
Thanks and Best Regards…
Part Number: CDCE6214 Hi guys,
I'm bringing up a new design where the CDCE6214 is programmed over USB. The Microchip MCP2221A acts as an USB-I2C bridge.
We have a CDCE6214-Q1EVM dev kit that can be used to validate output signals and generate a memory…
Part Number: CDCE6214-Q1EVM Hi Team,
We are using TICS Pro + CDCE6214-Q1EVM for testing. And we have some questions.
1. If we set OUT1 = LVDS 150MHz clk and set 25MHz PFD, 0.25%. How should I calculate spread frequency?
2. When I change output LVDS clk…