Part Number: CDCE937 Hi support team.
Regarding data byte 01, is it okay to overwrite bit6 (EEPROM Programin Status (read-only))?
Data byte 00 consists of only read only bits and the data sheet also prohibits writing, so I would like to confirm.
Also…
Part Number: CDCE937 Other Parts Discussed in Thread: CDCEL9XXPROGEVM , Hello,
I've just used the CDCEL9XXPROGEVM board to program a CDCE937 clock generator. I'd like to verify it successfully generates the expected clock outputs and its overall performance…
Part Number: CDCE937 I want to use the CDCE937 to generate four output clocks that will need to be in phase will each other.
27MHz in, 27MHZ, 148.5MHz, 200MHz and 212.5MHZ out. I see from the design tool that these clock can be generated with a zero ppm…
Part Number: CDCE937-Q1 Other Parts Discussed in Thread: TDA4VM Hello Expert.
Currently , I am checking CDCEC937 config of TDA4VM. I have questions about 'EELOCK' value.
Q1. If this value is 1 , written value is temporary (the values is returned…
Part Number: CDCE937 Other Parts Discussed in Thread: CDCE949 , CDCE925 , CDCE913 I am using CDCE937 for a new design. I want to use this part to generate 6 frequencies total, 2 frequencies per PLL using the associated dividers. My questions are as follows…
Part Number: CDCE937-Q1 Other Parts Discussed in Thread: CDCE937 Hi experts,
I want to get the configration of CDCE937QPWRQ1 under below condition:
xtal-load-pf = 3pF
input Xtal = 25MHz
output Y1-Y7 = 50MHz
spread-spectrum = normal
Can you provide the register…