Part Number: CDCEL913 Other Parts Discussed in Thread: AM5728 , , CDCE913 Hello,
In our Custom Board (AM5728 ) we are using cdcel913 chip for clock generation and it is interface using I2C.
I'm using VxWorks OS , I want to configure the this but I unable…
Part Number: CDCEL913 Other Parts Discussed in Thread: CDCEL9XXPROGEVM I saw in the datasheet (and in a previous Forum thread) that the "safe" number of EEPROM write cycles that may be performed is 1000; the same Forum thread mentioned that you can perform…
Hi Noel,
I am the FAE who supports Pateo, we don’t have to worry about the related settings of FPDLINK, and now I want to help customers confirm whether CDCEL913 can be configured with Y1 to output 192mhz and Y2 to output 184mhz.
Noel Fung said…
Part Number: CDCEL913 Hi team, I have a question about CDCEL913PW.
This device is programable and can TI write date which customers make before shipping?
Part Number: CDCEL913-Q1 Other Parts Discussed in Thread: CDCEL913 Hi TI,
CDCEL913 s upports n onvolatile EEPROM programming, but i can not find how to modify default EEPROM configuration. Could you help give some advice?
eg: I want to set default eeprom…
Part Number: CDCEL913 Hi, support team
My customer has the questions as follow:
I am using CDCEL913. I can output integer frequency, such as 33MHz However, once there are decimals, such as 32.768 MHz, the output is incorrect. For example, I set 32.768MHz…
Part Number: CDCEL913-Q1 Hi team
The crystal matching test result of CDCEL913-Q1 does not meet the customer requirements while customer could adjust the internal capacitance value of CDCEL913-Q and then meet the matching test, the test details we do not…
Part Number: CDCEL913 Hello Expert, I have questions regarding CDCEL913 as following. Would you answer it?
Datasheet said recommended crystal input freq ranege is up to 32MHz. But there isn't freq range regarding VCXO. Does it mean I can use higher frequency…
Part Number: CDCEL913 Other Parts Discussed in Thread: CLOCKPRO , , CODELOADER , USB2ANY Dear,
I want to use ClockPro to generate 24MHz clock setting for CDCEL913. However, after I sending Byte 27, CDCEL913 returns to default value, bypass the input crystal…