Part Number: CDCLVC1110 Other Parts Discussed in Thread: LMK00101 , CDCLVC1310 hi Experts
do TI have p2p solution against 5PB1110NDGI8?
I check the datasheet in 5PB11xx family
find5PB1110NDGI8 is VFQFPN package . and CDCLVC11xx family only have TSS…
Part Number: CDCLVC1110 Hello team,
Is it possible to use the CDCLVC1110 as a data line buffer instead of using it as a clock buffer where the d uty cycle is not critical?
Regards, Carlo
Part Number: CDCLVC1110 Other Parts Discussed in Thread: CDCLVC1102 What is the maximum capacitive load it can drive? ,
My design has a clock generator on one board whose output is connected to the CDCLVC1102 and the CDCLVC1102 output is connected to another…
Part Number: CDCLVC1110
Hi Team,
The customer is using CDCLVC1110. For the CDCLVC1110 datasheet, there are some errors.
1. Pin Configuration diagram Pin Number 10 is Y9 while in Pin Functions table Pin Number 10 is Y8 and Y9 does not have the corresponding…
Part Number: CDCLVC1110 Hello support team,
I have a question regarding CDCLVC11xx.
- Can CDCLVC11xx drive a CMOS IC (Vcc = 3.3 V) whose input capacitance is 20 pF with 50 MHz clock signal?
The period of 50 MHz clock signal is 20 ns. So I think the minimum…
Other Parts Discussed in Thread: CDCLVC1110 , CDCLVC1102 Hi Team,
is the CDCLVC1110 able to drive a 100CM tracelength at 40 MHz with 4mil traces with 4 mil spacing?
BR,
Lucas McKeehan
I am discussing on the MDC line.
Can i use an IC with part number CDCLVC1110. With this i can drive the MDC line from the processor to all the Slave devices.
Plz ignore "operate independently". It is fine even if some slaves see the clock signal…
Other Parts Discussed in Thread: CDCLVC1110 , SN74AUC1G17 Dear E2E Community,
In one of the application we are using reset fan out buffer, please suggest me to select the part number for the below requirement.
Input Channel :1
Output channel :Many
Voltage…