Part Number: CDCLVC1310 Hi,
Customer request the DPA report for CDCLVC1310RHBR and CDCV304PWR, the reprot include t est items, test methods, test results, conclusions and so on,
We can't search in the TI website, please kindly support, thanks.
Part Number: CDCLVC1310 Hello
1、schematic check
We use CDCLVC1310 as CLK BUFFER,The clock input and output circuits are shown in the following figure,please help check if the circuit is correct.
The detailed information of the circuit is as follows…
Part Number: CDCLVC1310 Hi TI Teams,
Can u help to check the schematic of CDCLVC1310? The schematic is as below.
CDCLVC1310RHBR SCH.pdf
Thanks,
Kind Regards
Part Number: CDCLVC1310 Hi Expert,
my customer is using CDCLVC1310 in server mother board, as single-end LVCMOS 50MHz input and output for FPGA system reference clock, but we don't find the input slew rate in datasheet, could you help to check it? thanks…
Part Number: CDCLVC1310-EVM I am using the CDCLVC1310-EVM. I am supplying 3.3V to both VDD and VDDO. I'm using the onboard 25MHz crystal oscillator to measure a square waveform, but am just getting a saw function instead. The output also varies from …
Part Number: CDCLVC1310-EVM Hi team,
One of our customers needs the design files or gerber files for the CDCLVC1310-EVM, are there any files available to the customer?
If not, could you please give some PCB layout guides such as capacitor placement, PCB board…
Part Number: CDCLVC1310 I'd like to use the CDCLVC1310 in a design I'm updating due to part availability. I'm interested in this device due to low additive jitter; a requirement. Also it has LVCMOS outputs; another requirement.
My VCTCXO has…
Part Number: CDCLVC1310 Dear team,
I cannot find the ESD rating data from device datasheet.
Could you share ESD information with us?
According to datasheet description, "these devices have limited built-in ESD protection"
Does that mean we…
Part Number: CDCLVC1310 Hi ,
One of my customer is using CDCLVC1310 .
They Doc1.docx are connecting LVCMOS (3.3V) to PRI_INP (pin#13).
PRI_INN is just connected with 1K pull up and pull down.
As per figure-3 in datasheet, they have mentioned 100 ohm pull…