Part Number: CDCM9102EVM Other Parts Discussed in Thread: CDCM9102 , CDCE6214 Hello,
I'm very interested in this product but I need to generate clock signal at 125 MHz and not 100 MHz. Is there a way to modify the frequency of the outputs ?
Or does…
Thank you very much for the information. If I buy one of CDCE62005EVM and CDCM9102EVM as clock generator, can I run it without needing to buy anything else?
Part Number: CDCM9102EVM Hello team,
My Customer is starting to evaluation CDCM9102EVM and he checks EVM User’s Guide.
It is hard to see the schematics, due to schematic is low-resolution.
Could you please share us the high-resolution schematic…
Hi Lane,
Thank you for the reply. I understood that input from external oscillator is supported in CDCM9102. But I'm little confused about information in "CDCM9102EVM Clock Evaluation Module User's Guide". In page.4 "5.2 Configuring a Single…
Hello Tamio,
I couldn't find the exact pullup resistance value from internal documentation but I believe that OS1 and OS0 indeed have pullup resistors. This is deducted by looking at the EVM schematic. The external pullup resistors for both pins are not…
Hello,
please see attached a clear version of the schematic.
/cfs-file/__key/communityserver-discussions-components-files/48/5852.CDCM9102EVM_5F00_schematic1.pdf
If the outputs are configured to LVDS please terminate with 100 ohm differential.
If LVPECL…