Part Number: CSD13380F3 Hi Team
do we have such automotive solution for FS03MR12A6MA1B?
below is datasheet.
https://www.infineon.com/dgdl/Infineon-FS03MR12A6MA1B-DataSheet-v01_00-EN.pdf?fileId=5546d4627862c3e501787e48f6ef330c
BRs
Brian
Part Number: CSD13380F3 Other Parts Discussed in Thread: CSD13381F4 , Why is the part CSD13380F3 in PSpice for TI software different with the package in datasheet. In the PSpice for TI,the Pin 1 is source, the Pin 2 is gate, Pin 3 is drain, as show in picture…
Part Number: CSD13380F3
We are constructing a circuit as shown below(please ignore the MAX4166 circuit on the left as we already isolated out from FemtoFET circuit).
VG1 is a function gen to generate a series of pulses to enable/disable FemtoFET while…
Part Number: CSD13380F3 Hi team,
my customer designing a nono-power device and have been using the CSD13380F3 N-Channel MOSFET with great success due to its low leakage. The datasheet says it has a max leakage of 25nA GS at 8V and 50nA SD at 9.6V. I'm…
Part Number: CSD13380F3 The datasheet specify max IDSS and IGSS only at 25degC. I need to know the max value at 0 to 50 (or 40) degC.
And if you have tips about other tiny NMOS and PMOS with even lower leakage that would be welcome too.
Part Number: CSD13380F3 Other Parts Discussed in Thread: CSD13385F5 Hi Team,
customers are looking for discrete NMOS type power MOS.
The Rdson is better below 5mhom and VDS is 8V~10V.
Package is 2*2mm2, does TI have any recommendation?
Thanks!
Patty …
Part Number: CSD13380F3 Dear all,
I would like to ask about this device.
The following phenomenon was reported by our customers.
As shown in the figure below, when the gate and drain voltages were measured with the source open, the gate was 45 mV and…
Part Number: BQ21040 Other Parts Discussed in Thread: TPS61288 , CSD13380F3 , , TPS22959 , BQ2980
Hello,
I am very new to this, but would like to get your help and build up my knowledge.
My Application is to make portable escape room puzzles that has on…
Part Number: CSD13380F3 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models Is noise modeled correctly in the Web TINA SPICE model? i.e. Does it match the real device?
Part Number: CSD13306W Other Parts Discussed in Thread: CSD25310Q2 , CSD17483F4 , CSD13380F3 , TINA-TI In the attached picture, CSD13306W is the NMOS model and CSD25310Q2 is the PMOS model. PMOS switches are in SSR configuration. The circuit is such that…