Part Number: CSD15380F3 Other Parts Discussed in Thread: CSD13385F5 , CSD13380F3
Hi,
The drain to source current leakage is 50nA maximum at 25C; however I would like to understand how this changes at 125 degC ambient; can you comment? Also which TI…
Part Number: CSD15380F3 Other Parts Discussed in Thread: CSD13385F5 , CSD13380F3 Hi Team,
We see that it gives the max leakage current for the drain to source as 50nA at 25C but I've come to understand that sometimes the current value under the max…
Hello Pragash,
Thanks for the inquiry. As Clemens has pointed out, TI has many analog switch products. I am the applications engineer for the power MOSFET product line. How much current does the signal require? Is this a small signal application or…
Eric,
The important spec is IDSS when VDS is applied and VGS is zero. It is not searchable on the distributor websites. It roughly scales with VDS voltage rating. A "good" FET shows 1uA or less. TI has the CSD13380F3 from the FemtoFET family, for example…
Other Parts Discussed in Thread: CSD13380F3 , CSD83325L Hi!
I am designing BMS design for research purpose. for that i cannot explain the whole idea but i need to control the charging and discharging of single lithium ion cell.
For this purpose i…
Hi Bhargav,
TI has many lower leakage devices in a variety of packages. Our lowest leakage FETs are: CSD15380F3 (20V), CSD13380F3 (12V) and CSD13385F5 (12V). These are tiny and can conduct between 0.5A and 3A maximum current. The CSD16570Q5B is our…
Cafain,
Thanks for posting.
We do not have a device that meets your exact requirements.
We can offer:
1. A device like the CSD13380F3 that has 2Vgs drive capability but is high for Ciss (120pF typical vs target <50pF).
2. A device like the CSD15380F3…
My apologies, these FETs do have low charge but you may want to check out the CSD15380F3 , CSD13380F3 and the CSD25480F3, these have lower charge still. FYI these are all silicon wafer level style packages.
All the devices discussed have a relatively…
Part Number: CSD15380F3 Other Parts Discussed in Thread: CSD13380F3 I have a new design I'm debugging that uses the csd15380f3 in two different places, one of which works and one of which doesn't. Can you take a look at my two applications and see if…
Part Number: CC3200 Hi, I'm trying to create my custom PCB using the CC3200R1M1RGCR and the XDS100v3 debugger.
I've posted my schematic here.
myPCBv0.1.pdf
I placed PFET for reverse battery protection. I use a 9V battery.
I use a buck converter…