Part Number: CSD17571Q2 Hello,
I am concerned about the increase in temperature of a MOSFET.
Example:
Temperature = 25 grad
I drive a power resistor, with a single pulse with ton=300ms; the current is 7A.
From the datasheet I extract Zth=0,2*190=38K/W…
Part Number: CSD17571Q2 Hi team,
It is nice to know you here. I want to penetrate CSD17571Q2 to my customer to do Active Mille CLAMP function, the circuit should be like below. The Vs may some 200ns pulse and the peak voltage should lower than 2V or even…
Part Number: CSD17571Q2 Other Parts Discussed in Thread: SN74AVC16T245
Is there a simple circuit to drive the gate control of an N-channel NexFET like the CSD17571Q2 when used as a 19V/4A load switch?
The on/off control signal is a 3.3V output from a…
Part Number: LM5050-1-Q1 Other Parts Discussed in Thread: LM74700-Q1 , , CSD17571Q2 , LM5050-1 ALL HI!
What is the difference between lm5050 and lm74700-q1 in use function? Whether it can be used interchangeably. My use requirements are: 1. Prevent the reverse…
Part Number: LM25118 Hello,
Minor question, for the linked webbench design would it be acceptable to replace the CSD17571Q2 in the design with the CSD17327Q5A and the FSV360FP with the STPS10M60SF ?
PDF of WebBench Design
Image of Design
Other Parts Discussed in Thread: LMG1020 , CSD17571Q2 , CSD15571Q2 , CSD16301Q2 Dear sir ,
i want to create a signal from Arduino Due at 5MHZ (a square wave ) 50% duty cycle to be connected to fast gate controlled mosfet(NPN) to switch a load 12 volt 1 …
Part Number: CSD19538Q2 Other Parts Discussed in Thread: CSD16301Q2 , CSD17571Q2 , Hi,
My customer need below auto grade MOS. please kindly recommend accordingly. thanks.
CSD16301Q2_25V_5A_TI
CSD17571Q2_30V_22A_TI
CSD19538Q2_100V_14.4A_TI
…
Part Number: BQ24171 Other Parts Discussed in Thread: CSD17571Q2 , CSD17313Q2 , Hi I have two questions.
1.Please tell me how to select ACFET and RBFET.
2.Also, please tell us the reason for selecting the ACFET and BRFET used in the evaluation board.
Please…
Hi Dan,
Thanks for reaching out. Yes, the FemtoFETs can be difficult to hand solder. I'm including a link below to the FemtoFET SMT guidelines that include some instructions on rework. FET packages that may be easier to hand solder include the SON packages…
Part Number: LM5175 Other Parts Discussed in Thread: CSD19538Q2 , CSD17571Q2 , , LM5176 Hi ,
Please see attached simulated design using Webench for Lm5175 . On our board we changed the FET on Boost side from CSD19538Q2 to CSD17571Q2 and the system has stopped…